In case of using two DM816Xs on a board, is there way to implement "shared memory" between the two DM816Xs?
How can we use shared memory between the two DM816Xs?
Yes, this can be done through PCIe interface. This is only way we could share memory between 2 DM8167 devices
Karthik Swaminathan