Linux Fast Boot: Only 560 milliseconds from reset to shell!

Hi, I glad to announce possible fastest Linux fast boot ever!

Only 560 milliseconds from reset to shell!

Works on DM365 EVM.

Boot log with timestamps

Logging starts at 20 ms from reset.

0.000 0.000: DM36x initialization passed! 
0.000 0.000: Optimized TI UBL 1.50 http://www.MakeLinux.com/emb/fastboot
0.010 0.010: Compiled on Jan 5 2011 at 02:38:56 with gcc 4.3.3
0.010 0.000: Starting NAND Copy...
0.479 0.469: length=0x00156000 DONE
0.479 0.000: Jumping to entry point at 0x80008000.
0.542 0.063: BusyBox v1.16.2 hush - the humble shell


You don't believe? You can find binary demo here: http://www.makelinux.com/emb/fastboot/ and try it by your self.

Please leave yours comments and feedback in this forum.


Constantine
Embedded Linux Consulting: http://www.MakeLinux.com/
Linux and TI DaVinci Technology Portal: http://www.Linux-DaVinci.info/

Please consider to   Verify the Answer   if applicable