A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L138Hello,
I have a flash connected to SPI0 in a custom board, I still do not detect its idcode ( FF FF FF...) , so I got buack to EVM to see if I can work with its SPI0, I also did not see any change in the CS when doing "sf probe 0:0", so I tried to work with the CCS and to look if I can detects its signal in scop : CLK, SIMO, CS and SOMI. I added to the GEL a simple pinmux:
SPI0_PINMUX
{
PSC0_LPSC_enable(0,LPSC_SPI0)
PINMUX3 = (PINMUX3 & ~0x~F000FF0F)| (0x10001101)
..
]
But I only see the clock, and the CS does not change. When using SPI1, I do see the CS changes value.
I wonder if you have any example, of working with SPI0 with OMAP-L138
Thank you very much,
Ran