Hi
I am running the IPNC software on a DVEVM board with the DM365.(both purchased and registered). I now want to achieve USB streaming video within the IPNC framework. So my questions are
1. Are the UVC drivers already present in the LSP or do i need to add them and rebuild the kernel? If i have to add,how do i go about it?
2. I also need to include a application to view the USB video in the application layer right?
3.Can i flash the linux image independent of the IPNC software on top? Can someone help me on this?
Thank you