Hello All,
I'm Just a Little freshman in the Filed of DSP processors
I have got My BeagleBoard Rev.A having DM3730 over it which i thought is fully Compatible with OMAP3530.
I want to acquire a signal form the Audio input over this board using the DSP.
I have searched the Internet and the ti.com and found a very useful example , seems to be exactly what i want to do in the following link
"http://processors.wiki.ti.com/index.php/OMAP-L137_Audio_Drivers_in_the_DSP_%2B_Linux"
Unfortunately i have got may problems the main points where:
1- That topic and the example shown their working over OMAP-L137 , not OMAP3530
2- The examples include some lib. like " ti.pspiom.platforms.codec" , "ti.pspiom.platforms.xxxxx.audio" and others.
Information about my system :
* I'm Using Linux machine as a host
* i have Angstrom , kernel 2.6.32
*dsplink_linux_1_65_00_03
*c6000_6.1.16_setup_linux_x86
So could anyone can help in that, I hope my question in not so noob
Thanks All in Advance