This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DM8168 EVM eth1 giga interface problem

Hi,

 

I'm using DM8168 DDR3 EVM Rev-C with daughter board (TMDXVSDC8168) and ezsdk 5.02.01.59.

My app's main function is receving data from eth0 and save it to SATA HDD and retransmitting to eth1.

eth0 is work well with gigabit ethernet, but eth1 is not.

When I boot EVM eth1 connected to a gigabit port, no data transmission occurred.

At this time I unplug the eth1 cable and plug to a 100M port, data transmission is occurred.

After data transmission is occurred, I connect eth1 to a giga port again, data transmission is work-well.

 

When EVM is booted with eth1 connected 100M port, all data transmission is no porblem.

More exactly explan is;

When boot eth1 with giga port, I check ifconfig command, some ethernet packets are received from eth1.

But, no data is transmitted from my app, also no ping reponse to eth1 from outside.

At this time, I run 'ifconfig eth1 down' and the EVM is hangged.

Before EVM is hannged, I do unplug eth1 cable from giga port and replug it to giga port again,

no data transmission.

 

Help me.

  • Hyunho Youn

    Can you provide kernel boot logs with eth1 connected with 1G and 100M.

    with regards

    Mugunthan V N

     

  • In reply to Mugunthan V N:

    Dear Mugunthan V N,

     

    Thank you for your reply.

     

    Before attaching the logs, I tell some more information.

    After posting this question, I tested the other daughter board rented by my local distributer.

    I got the same result, so this problem might be related with kernel.

     

    with regards

    Hyunho Youn

     

    Log 1. boot with giga-port

    --------------------------------------------------------------------------------------------
    Loading from nand0, offset 0x200000
       Image Name:   Linux-2.6.37
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2840476 Bytes = 2.7 MiB
       Load Address: 80008000
       Entry Point:  80008000
    bootargs :: 'console=ttyO2,115200n8 mem=256M root=/dev/mtdblock12 rw rootfstype=yaffs2 MAC0=00:30:6F:F2:F2:F3 MAC1=00:30:6F:F2:F2:F4'
    ## Booting kernel from Legacy Image at 81000000 ...
       Image Name:   Linux-2.6.37
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2840476 Bytes = 2.7 MiB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.
    Linux version 2.6.37 (
    h2y@wolf) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #40 Wed Nov 9 10:43:58 KST 2011
    CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
    CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
    Machine: ti8168evm
    reserved size = 52428800 at 0
    FB: Reserving 52428800 bytes SDRAM for VRAM
    Memory policy: ECC disabled, Data cache writeback
    OMAP chip is TI8168 1.1
    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 52224
    Kernel command line: console=ttyO2,115200n8 mem=256M root=/dev/mtdblock12 rw rootfstype=yaffs2 MAC0=00:30:6F:F2:F2:F3 MAC1=00:30:6F:F2:F2:F4
    PID hash table entries: 1024 (order: 0, 4096 bytes)
    Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
    Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    Memory: 206MB = 206MB total
    Memory: 202648k/202648k available, 59496k reserved, 0K highmem
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
        DMA     : 0xffc00000 - 0xffe00000   (   2 MB)
        vmalloc : 0xd0800000 - 0xf8000000   ( 632 MB)
        lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
        modules : 0xbf000000 - 0xc0000000   (  16 MB)
          .init : 0xc0008000 - 0xc003d000   ( 212 kB)
          .text : 0xc003d000 - 0xc0560000   (5260 kB)
          .data : 0xc0560000 - 0xc05a9f80   ( 296 kB)
    SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    NR_IRQS:407
    IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    Total of 128 interrupts on 1 active controller
    GPMC revision 6.0
    Trying to install interrupt handler for IRQ400
    Trying to install interrupt handler for IRQ401
    Trying to install interrupt handler for IRQ402
    Trying to install interrupt handler for IRQ403
    Trying to install interrupt handler for IRQ404
    Trying to install interrupt handler for IRQ405
    Trying to install interrupt handler for IRQ406
    Trying to install type control for IRQ407
    Trying to set irq flags for IRQ407
    OMAP clockevent source: GPTIMER1 at 27000000 Hz
    Console: colour dummy device 80x30
    Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
    pid_max: default: 32768 minimum: 301
    Security Framework initialized
    Mount-cache hash table entries: 512
    CPU: Testing write buffer coherency: ok
    devtmpfs: initialized
    omap_voltage_early_init: voltage driver support not added
    regulator: core version 0.5
    regulator: dummy:
    NET: Registered protocol family 16
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    omap_mux_init: Add partition: #1: core, flags: 0
    _omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl
    _omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda
    NOR: Can't request GPMC CS
    registered ti816x_vpss device
    registered ti816x_gpio_vr device
    registered TI816x on-chip HDMI device
    registered ti816x_sr device
    pm_dbg_init: only OMAP3 supported
    Registered ti81xx_fb device
    ti816x_pcie: Invoking PCI BIOS...
    ti816x_pcie: Setting up Host Controller...
    ti816x_pcie: Register base mapped @0xd0820000
    ti816x_pcie: Starting PCI scan...
    PCI: bus0: Fast back to back transfers enabled
    bio: create slab <bio-0> at 0
    regulator: VFB: 800 <--> 1025 mV at 920 mV
    vgaarb: loaded
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
    omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz
    Advanced Linux Sound Architecture Driver Version 1.0.23.
    cfg80211: Calling CRDA to update world regulatory domain
    Switching to clocksource gp timer
    musb-hdrc: version 6.0, host, debug=0
    musb-hdrc musb-hdrc.0: dma type: dma-cppi41
    registerd cppi-dma Intr @ IRQ 17
    Cppi41 Init Done
    musb-hdrc: kernel must blacklist external hubs
    musb-hdrc musb-hdrc.0: MUSB HDRC host driver
    musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
    usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb1: Product: MUSB HDRC host driver
    usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
    usb usb1: SerialNumber: musb-hdrc.0
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    musb-hdrc musb-hdrc.0: USB Host mode controller at d080c000 using DMA, IRQ 18
    musb-hdrc musb-hdrc.1: dma type: dma-cppi41
    musb-hdrc: kernel must blacklist external hubs
    musb-hdrc musb-hdrc.1: MUSB HDRC host driver
    musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
    usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb2: Product: MUSB HDRC host driver
    usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
    usb usb2: SerialNumber: musb-hdrc.1
    hub 2-0:1.0: USB hub found
    hub 2-0:1.0: 1 port detected
    musb-hdrc musb-hdrc.1: USB Host mode controller at d081e800 using DMA, IRQ 19
    NET: Registered protocol family 2
    IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
    TCP established hash table entries: 8192 (order: 4, 65536 bytes)
    TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
    TCP: Hash tables configured (established 8192 bind 8192)
    TCP reno registered
    UDP hash table entries: 256 (order: 0, 4096 bytes)
    UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    NET: Registered protocol family 1
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    PMU: registered new PMU device of type 0
    omap-iommu omap-iommu.0: ducati registered
    omap-iommu omap-iommu.1: sys registered
    JFFS2 version 2.2. (NAND) Aⓒ 2001-2006 Red Hat, Inc.
    msgmni has been set to 395
    Block layer SCSI generic (bsg) driver version 0.4 loaded (major 254)
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
    omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
    console [ttyO2] enabled
    brd: module loaded
    loop: module loaded
    ahci ahci.0: forcing PORTS_IMPL to 0x3
    ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
    ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc
    scsi0 : ahci_platform
    scsi1 : ahci_platform
    ata1: SATA max UDMA/133 irq_stat 0x00400040, connection status changed irq 16
    ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
    omap2-nand driver initializing
    NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron )
    Creating 14 MTD partitions on "omap2-nand.0":
    0x000000000000-0x000000100000 : "bootloader"
    0x000000100000-0x000000180000 : "params"
    0x000000180000-0x000000200000 : "syft"
    0x000000200000-0x000000600000 : "ki"
    0x000000600000-0x000000a00000 : "ri"
    0x000000a00000-0x000002200000 : "si"
    0x000002200000-0x000002c00000 : "wi"
    0x000002c00000-0x000002d00000 : "ci"
    0x000002d00000-0x000002e00000 : "5i"
    0x000002e00000-0x000002f00000 : "6i"
    0x000002f00000-0x000003300000 : "7i(initrd)"
    0x000003300000-0x000009700000 : "rootfs 1"
    0x000009700000-0x00000fb00000 : "rootfs 2"
    0x00000fb00000-0x000010000000 : "zzogary"
    davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
    davinci_mdio davinci_mdio.0: detected phy mask fffffff9
    davinci_mdio.0: probed
    davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
    davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver unknown
    PPP generic driver version 2.4.2
    PPP Deflate Compression module registered
    PPP BSD Compression module registered
    usbcore: registered new interface driver cdc_ether
    usbcore: registered new interface driver dm9601
    Initializing USB Mass Storage driver...
    usbcore: registered new interface driver usb-storage
    USB Mass Storage support registered.
    mice: PS/2 mouse device common for all mice
    i2c /dev entries driver
    Linux video capture interface: v2.00
    usbcore: registered new interface driver uvcvideo
    USB Video Class driver (v1.0.0)
    OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
    md: raid1 personality registered for level 1
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    usbcore: registered new interface driver snd-usb-audio
    asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
    ALSA device list:
      #0: TI81XX EVM
    GACT probability NOT on
    Mirror/redirect action on
    netem: version 1.2
    TCP cubic registered
    NET: Registered protocol family 10
    lo: Disabled Privacy Extensions
    NET: Registered protocol family 17
    lib80211: common routines for IEEE802.11 drivers
    VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    omap_voltage_late_init: Voltage driver support not added
    smartreflex smartreflex: Driver is not initialized, nTarget values are not found
    regulator_init_complete: disabling VFB
    EMAC Address = 00:30:6F:F2:F2:F3
    EMAC Address = 00:30:6F:F2:F2:F4
    ata2: SATA link down (SStatus 0 SControl 300)
    ata1: link is slow to respond, please be patient (ready=0)
    ata1: softreset failed (device not ready)
    ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
    ata1.00: ATA-7: ST3250310CS, 3.ACD, max UDMA/133
    ata1.00: 488397168 sectors, multi 0: LBA48 NCQ (depth 31/32)
    ata1.00: configured for UDMA/133
    scsi 0:0:0:0: Direct-Access     ATA      ST3250310CS      3.AC PQ: 0 ANSI: 5
    sd 0:0:0:0: Attached scsi generic sg0 type 0
    sd 0:0:0:0: [sda] 488397168 512-byte logical blocks: (250 GB/232 GiB)
    sd 0:0:0:0: [sda] Write Protect is off
    sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
     sda: sda1 sda2
    sd 0:0:0:0: [sda] Attached SCSI disk
    md: Waiting for all devices to be available before autodetect
    md: If you don't use raid, use raid=noautodetect
    md: Autodetecting RAID arrays.
    md: Scanned 0 and added 0 devices.
    md: autorun ...
    md: ... autorun DONE.
    yaffs: dev is 32505868 name is "mtdblock12" rw
    yaffs: passed flags ""
    VFS: Mounted root (yaffs2 filesystem) on device 31:12.
    devtmpfs: mounted
    Freeing init memory: 212K
    INIT: version 2.88 booting
    Mount tmpfs on /tmp
    nflashdd: Assume mtd2 as syft
    nflashdd Init OK!

                            Welcome to Embedded Linux

    devpts: called with bogus options
    EXT3-fs: barriers not enabled
    kjournald starting.  Commit interval 5 seconds
    EXT3-fs (sda1): using internal journal
    EXT3-fs (sda1): mounted filesystem with writeback data mode
    Initialize SI ... [  OK  ]
    Setting hostname NVR Alpha [  OK  ]
    davinci_mdio davinci_mdio.0: resetting idled controller
    net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f014)
    ADDRCONF(NETDEV_UP): eth0: link is not ready
    net eth1: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:02, id=282f014)
    ADDRCONF(NETDEV_UP): eth1: link is not ready
    PHY: 0:01 - Link is Up - 1000/Full
    ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    PHY: 0:02 - Link is Up - 1000/Full
    ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
    sy_misc Init OK!


    NVR login: root
    Password:
    [NVR ~]# ifconfig
    eth0      Link encap:Ethernet  HWaddr 00:30:6F:F2:F2:F3
              inet addr:10.10.213.122  Bcast:10.10.255.255  Mask:255.255.0.0
              inet6 addr: fe80::230:6fff:fef2:f2f3/64 Scope:Link
              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
              RX packets:66662 errors:0 dropped:0 overruns:0 frame:0
              TX packets:37273 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:1000
              RX bytes:90117415 (85.9 MiB)  TX bytes:2465496 (2.3 MiB)
              Interrupt:40 Base address:0x8000

    eth1      Link encap:Ethernet  HWaddr 00:30:6F:F2:F2:F4
              inet addr:192.168.213.122  Bcast:192.168.255.255  Mask:255.255.0.0
              inet6 addr: fe80::230:6fff:fef2:f2f4/64 Scope:Link
              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
              RX packets:135 errors:0 dropped:0 overruns:0 frame:0
              TX packets:6 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:1000
              RX bytes:8603 (8.4 KiB)  TX bytes:468 (468.0 B)
              Interrupt:44 Base address:0x8000

    lo        Link encap:Local Loopback
              inet addr:127.0.0.1  Mask:255.0.0.0
              inet6 addr: ::1/128 Scope:Host
              UP LOOPBACK RUNNING  MTU:16436  Metric:1
              RX packets:114 errors:0 dropped:0 overruns:0 frame:0
              TX packets:114 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:0
              RX bytes:10714 (10.4 KiB)  TX bytes:10714 (10.4 KiB)

    [NVR ~]# ping 192.168.213.95
    PING 192.168.213.95 (192.168.213.95): 56 data bytes

    --- 192.168.213.95 ping statistics ---
    33 packets transmitted, 0 packets received, 100% packet loss

    [NVR ~]#
    [NVR ~]# PHY: 0:02 - Link is Down             <--- change LAN port from giga-port to 100M port
    PHY: 0:02 - Link is Up - 100/Full

    [NVR ~]#
    [NVR ~]# ping 192.168.213.95
    PING 192.168.213.95 (192.168.213.95): 56 data bytes
    64 bytes from 192.168.213.95: seq=0 ttl=64 time=5.801 ms
    64 bytes from 192.168.213.95: seq=1 ttl=64 time=0.295 ms
    64 bytes from 192.168.213.95: seq=2 ttl=64 time=0.316 ms
    64 bytes from 192.168.213.95: seq=3 ttl=64 time=0.466 ms
    64 bytes from 192.168.213.95: seq=4 ttl=64 time=0.202 ms
    64 bytes from 192.168.213.95: seq=5 ttl=64 time=0.275 ms
    64 bytes from 192.168.213.95: seq=6 ttl=64 time=0.223 ms
    64 bytes from 192.168.213.95: seq=7 ttl=64 time=0.280 ms
    PHY: 0:02 - Link is Down             <--- change LAN port from 100M port to giga-port
    PHY: 0:02 - Link is Up - 1000/Full
    64 bytes from 192.168.213.95: seq=21 ttl=64 time=0.255 ms
    64 bytes from 192.168.213.95: seq=22 ttl=64 time=0.277 ms
    64 bytes from 192.168.213.95: seq=23 ttl=64 time=0.307 ms
    64 bytes from 192.168.213.95: seq=24 ttl=64 time=0.659 ms
    64 bytes from 192.168.213.95: seq=25 ttl=64 time=0.477 ms
    64 bytes from 192.168.213.95: seq=26 ttl=64 time=0.267 ms
    64 bytes from 192.168.213.95: seq=27 ttl=64 time=1.451 ms
    64 bytes from 192.168.213.95: seq=28 ttl=64 time=0.222 ms

    --- 192.168.213.95 ping statistics ---
    29 packets transmitted, 16 packets received, 44% packet loss
    round-trip min/avg/max = 0.202/0.735/5.801 ms

    [NVR ~]#

     

     

    Log 2. boot with 100M port

    --------------------------------------------------------------------------------------------
    Loading from nand0, offset 0x200000
       Image Name:   Linux-2.6.37
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2840476 Bytes = 2.7 MiB
       Load Address: 80008000
       Entry Point:  80008000
    bootargs :: 'console=ttyO2,115200n8 mem=256M root=/dev/mtdblock12 rw rootfstype=yaffs2 MAC0=00:30:6F:F2:F2:F3 MAC1=00:30:6F:F2:F2:F4'
    ## Booting kernel from Legacy Image at 81000000 ...
       Image Name:   Linux-2.6.37
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2840476 Bytes = 2.7 MiB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.
    Linux version 2.6.37 (h2y@wolf) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #40 Wed Nov 9 10:43:58 KST 2011
    CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
    CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
    Machine: ti8168evm
    reserved size = 52428800 at 0
    FB: Reserving 52428800 bytes SDRAM for VRAM
    Memory policy: ECC disabled, Data cache writeback
    OMAP chip is TI8168 1.1
    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 52224
    Kernel command line: console=ttyO2,115200n8 mem=256M root=/dev/mtdblock12 rw rootfstype=yaffs2 MAC0=00:30:6F:F2:F2:F3 MAC1=00:30:6F:F2:F2:F4
    PID hash table entries: 1024 (order: 0, 4096 bytes)
    Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
    Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    Memory: 206MB = 206MB total
    Memory: 202648k/202648k available, 59496k reserved, 0K highmem
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
        DMA     : 0xffc00000 - 0xffe00000   (   2 MB)
        vmalloc : 0xd0800000 - 0xf8000000   ( 632 MB)
        lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
        modules : 0xbf000000 - 0xc0000000   (  16 MB)
          .init : 0xc0008000 - 0xc003d000   ( 212 kB)
          .text : 0xc003d000 - 0xc0560000   (5260 kB)
          .data : 0xc0560000 - 0xc05a9f80   ( 296 kB)
    SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    NR_IRQS:407
    IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    Total of 128 interrupts on 1 active controller
    GPMC revision 6.0
    Trying to install interrupt handler for IRQ400
    Trying to install interrupt handler for IRQ401
    Trying to install interrupt handler for IRQ402
    Trying to install interrupt handler for IRQ403
    Trying to install interrupt handler for IRQ404
    Trying to install interrupt handler for IRQ405
    Trying to install interrupt handler for IRQ406
    Trying to install type control for IRQ407
    Trying to set irq flags for IRQ407
    OMAP clockevent source: GPTIMER1 at 27000000 Hz
    Console: colour dummy device 80x30
    Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
    pid_max: default: 32768 minimum: 301
    Security Framework initialized
    Mount-cache hash table entries: 512
    CPU: Testing write buffer coherency: ok
    devtmpfs: initialized
    omap_voltage_early_init: voltage driver support not added
    regulator: core version 0.5
    regulator: dummy:
    NET: Registered protocol family 16
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    omap_mux_init: Add partition: #1: core, flags: 0
    _omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl
    _omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda
    NOR: Can't request GPMC CS
    registered ti816x_vpss device
    registered ti816x_gpio_vr device
    registered TI816x on-chip HDMI device
    registered ti816x_sr device
    pm_dbg_init: only OMAP3 supported
    Registered ti81xx_fb device
    ti816x_pcie: Invoking PCI BIOS...
    ti816x_pcie: Setting up Host Controller...
    ti816x_pcie: Register base mapped @0xd0820000
    ti816x_pcie: Starting PCI scan...
    PCI: bus0: Fast back to back transfers enabled
    bio: create slab <bio-0> at 0
    regulator: VFB: 800 <--> 1025 mV at 920 mV
    vgaarb: loaded
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
    omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz
    Advanced Linux Sound Architecture Driver Version 1.0.23.
    cfg80211: Calling CRDA to update world regulatory domain
    Switching to clocksource gp timer
    musb-hdrc: version 6.0, host, debug=0
    musb-hdrc musb-hdrc.0: dma type: dma-cppi41
    registerd cppi-dma Intr @ IRQ 17
    Cppi41 Init Done
    musb-hdrc: kernel must blacklist external hubs
    musb-hdrc musb-hdrc.0: MUSB HDRC host driver
    musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
    usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb1: Product: MUSB HDRC host driver
    usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
    usb usb1: SerialNumber: musb-hdrc.0
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    musb-hdrc musb-hdrc.0: USB Host mode controller at d080c000 using DMA, IRQ 18
    musb-hdrc musb-hdrc.1: dma type: dma-cppi41
    musb-hdrc: kernel must blacklist external hubs
    musb-hdrc musb-hdrc.1: MUSB HDRC host driver
    musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
    usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb2: Product: MUSB HDRC host driver
    usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
    usb usb2: SerialNumber: musb-hdrc.1
    hub 2-0:1.0: USB hub found
    hub 2-0:1.0: 1 port detected
    musb-hdrc musb-hdrc.1: USB Host mode controller at d081e800 using DMA, IRQ 19
    NET: Registered protocol family 2
    IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
    TCP established hash table entries: 8192 (order: 4, 65536 bytes)
    TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
    TCP: Hash tables configured (established 8192 bind 8192)
    TCP reno registered
    UDP hash table entries: 256 (order: 0, 4096 bytes)
    UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    NET: Registered protocol family 1
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    PMU: registered new PMU device of type 0
    omap-iommu omap-iommu.0: ducati registered
    omap-iommu omap-iommu.1: sys registered
    JFFS2 version 2.2. (NAND) Aⓒ 2001-2006 Red Hat, Inc.
    msgmni has been set to 395
    Block layer SCSI generic (bsg) driver version 0.4 loaded (major 254)
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
    omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
    console [ttyO2] enabled
    brd: module loaded
    loop: module loaded
    ahci ahci.0: forcing PORTS_IMPL to 0x3
    ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
    ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc
    scsi0 : ahci_platform
    scsi1 : ahci_platform
    ata1: SATA max UDMA/133 irq_stat 0x00400040, connection status changed irq 16
    ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
    omap2-nand driver initializing
    NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron )
    Creating 14 MTD partitions on "omap2-nand.0":
    0x000000000000-0x000000100000 : "bootloader"
    0x000000100000-0x000000180000 : "params"
    0x000000180000-0x000000200000 : "syft"
    0x000000200000-0x000000600000 : "ki"
    0x000000600000-0x000000a00000 : "ri"
    0x000000a00000-0x000002200000 : "si"
    0x000002200000-0x000002c00000 : "wi"
    0x000002c00000-0x000002d00000 : "ci"
    0x000002d00000-0x000002e00000 : "5i"
    0x000002e00000-0x000002f00000 : "6i"
    0x000002f00000-0x000003300000 : "7i(initrd)"
    0x000003300000-0x000009700000 : "rootfs 1"
    0x000009700000-0x00000fb00000 : "rootfs 2"
    0x00000fb00000-0x000010000000 : "zzogary"
    davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
    davinci_mdio davinci_mdio.0: detected phy mask fffffff9
    davinci_mdio.0: probed
    davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
    davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver unknown
    PPP generic driver version 2.4.2
    PPP Deflate Compression module registered
    PPP BSD Compression module registered
    usbcore: registered new interface driver cdc_ether
    usbcore: registered new interface driver dm9601
    Initializing USB Mass Storage driver...
    usbcore: registered new interface driver usb-storage
    USB Mass Storage support registered.
    mice: PS/2 mouse device common for all mice
    i2c /dev entries driver
    Linux video capture interface: v2.00
    usbcore: registered new interface driver uvcvideo
    USB Video Class driver (v1.0.0)
    OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
    md: raid1 personality registered for level 1
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    usbcore: registered new interface driver snd-usb-audio
    asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
    ALSA device list:
      #0: TI81XX EVM
    GACT probability NOT on
    Mirror/redirect action on
    netem: version 1.2
    TCP cubic registered
    NET: Registered protocol family 10
    lo: Disabled Privacy Extensions
    NET: Registered protocol family 17
    lib80211: common routines for IEEE802.11 drivers
    VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    omap_voltage_late_init: Voltage driver support not added
    smartreflex smartreflex: Driver is not initialized, nTarget values are not found
    regulator_init_complete: disabling VFB
    EMAC Address = 00:30:6F:F2:F2:F3
    EMAC Address = 00:30:6F:F2:F2:F4
    ata2: SATA link down (SStatus 0 SControl 300)
    ata1: link is slow to respond, please be patient (ready=0)
    ata1: softreset failed (device not ready)
    ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
    ata1.00: ATA-7: ST3250310CS, 3.ACD, max UDMA/133
    ata1.00: 488397168 sectors, multi 0: LBA48 NCQ (depth 31/32)
    ata1.00: configured for UDMA/133
    scsi 0:0:0:0: Direct-Access     ATA      ST3250310CS      3.AC PQ: 0 ANSI: 5
    sd 0:0:0:0: Attached scsi generic sg0 type 0
    sd 0:0:0:0: [sda] 488397168 512-byte logical blocks: (250 GB/232 GiB)
    sd 0:0:0:0: [sda] Write Protect is off
    sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
     sda: sda1 sda2
    sd 0:0:0:0: [sda] Attached SCSI disk
    md: Waiting for all devices to be available before autodetect
    md: If you don't use raid, use raid=noautodetect
    md: Autodetecting RAID arrays.
    md: Scanned 0 and added 0 devices.
    md: autorun ...
    md: ... autorun DONE.
    yaffs: dev is 32505868 name is "mtdblock12" rw
    yaffs: passed flags ""
    VFS: Mounted root (yaffs2 filesystem) on device 31:12.
    devtmpfs: mounted
    Freeing init memory: 212K
    INIT: version 2.88 booting
    Mount tmpfs on /tmp
    nflashdd: Assume mtd2 as syft
    nflashdd Init OK!

                            Welcome to Embedded Linux

    devpts: called with bogus options
    EXT3-fs: barriers not enabled
    kjournald starting.  Commit interval 5 seconds
    EXT3-fs (sda1): using internal journal
    EXT3-fs (sda1): mounted filesystem with writeback data mode
    Initialize SI ... [  OK  ]
    Setting hostname NVR Alpha [  OK  ]
    davinci_mdio davinci_mdio.0: resetting idled controller
    net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f014)
    ADDRCONF(NETDEV_UP): eth0: link is not ready
    net eth1: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:02, id=282f014)
    ADDRCONF(NETDEV_UP): eth1: link is not ready
    PHY: 0:01 - Link is Up - 1000/Full
    ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    PHY: 0:02 - Link is Up - 100/Full
    ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
    sy_misc Init OK!


    NVR login: root
    Password:
    [NVR ~]# ping 192.168.213.95
    PING 192.168.213.95 (192.168.213.95): 56 data bytes
    64 bytes from 192.168.213.95: seq=0 ttl=64 time=22.235 ms
    64 bytes from 192.168.213.95: seq=1 ttl=64 time=0.782 ms
    64 bytes from 192.168.213.95: seq=2 ttl=64 time=0.187 ms
    64 bytes from 192.168.213.95: seq=3 ttl=64 time=0.297 ms
    64 bytes from 192.168.213.95: seq=4 ttl=64 time=0.188 ms
    64 bytes from 192.168.213.95: seq=5 ttl=64 time=0.280 ms
    64 bytes from 192.168.213.95: seq=6 ttl=64 time=0.260 ms
    64 bytes from 192.168.213.95: seq=7 ttl=64 time=0.363 ms
    64 bytes from 192.168.213.95: seq=8 ttl=64 time=0.191 ms

    --- 192.168.213.95 ping statistics ---
    9 packets transmitted, 9 packets received, 0% packet loss
    round-trip min/avg/max = 0.187/2.753/22.235 ms

    [NVR ~]#

     

     

     

     

  • In reply to Hyunho Youn:

    Hyunho Youn

    Please apply the patch below to enable giga bit tx clocking for the phy.

    http://arago-project.org/git/projects/linux-omap3.git?p=projects/linux-omap3.git;a=commit;h=3228b1d8e5270ee56002e7f59d839ed8b6b85606

    with regards

    Mugunthan V N

  • In reply to Mugunthan V N:

    Mugunthan V N

     

    Thanks you very much.

    My problem is solved by the patch.

     

    regards,

    Hyunho Youn

  • In reply to Mugunthan V N:

    Mugunthan V N,

      Do I understand correctly:

    1. This patch configures the PHY chip to output 125mhz clock on the tx_clk line when it is in giga bit mode?   
    2. To operate in Gigabit mode, the EMAC requires clock pulses on tx_clk line.  Does it matter frequency signal it gets?
    3. In my case (custom hardware), it only operates in gigabit mode, so the tx_clk signal is not attached to anything.  Do you think hooking the tx_clk input to any clock would be sufficient to work around the problem?

    Thanks,

      Ryan

  • In reply to Ryan Miller:

    Hi,

      To follow up.  Feeding the TX_CLK pin with just about any clock does allow the chip to enter Gigabit mode.  We have it hooked to a 13.5mhz timer output pin of Davinci.  So, this works if you only need gigabit mode. 

    Ryan

     

  • In reply to Ryan Miller:

    Hi,

     

    I tested my app on 8168 EVM.

    And I did not fix or change HW. I did apply the patch to kernel source.

    After kernel patch, 100M/Giga ethernet connection is working well. (switching 100M/Giga is ok)

    I'm not HW engineer, so I have nothing to tell you about HW.

     

    Regards.

  • In reply to Hyunho Youn:

    Hi,

      I'm glad the patch works for you.  From my understanding the patch works only for the EVM board, or probably any using the LSI ET1011 Gigabit PHY.  For my situation, we are using a different PHY (Micrel KSZ9021GN), which does not work with the patch.  My PHY does not have an option to output a clock on tx_clk lines when in gigabit mode.  So, I'm trying to find an alternative solution.  As I mentioned, at minimum we can hook the tx_clk line to a clock (instead of the PHY) and use only Gigabit mode.  I've verified this hack.  I'm still searching for a solution which allows 10/100/1000 Mbps operation.

    Thanks,

      Ryan 

  • In reply to Ryan Miller:

    Hi, Ryan!

    We have same PHY (KSZ9021GN) chip as you and it didn't work on our custom board not in any mode. (At u-boot stage I see error message: WARN: emac_send_packet: No link) But from u-boot command line I can read/write PHY registers (mii). Do you have any decision of your problem? May be it is help to me too. Thank you.

  • In reply to Mugunthan V N:

    Hi Mugunthan

    we also meet problem about net,

    we develop using dvrrdk 2.80 dm816x evm board,

    the problem is that if we connect 8168 board with PC through switch or router ,link is up and stability,

    if we connect PC and 8168 board directly ,the link is up and down all the time

    Print like
    Link is up

    Link is down ,

    and we test 4 Pc, only one is works well, other 3 Link is up and down all the time

    So how can net link not stability ?

    best regards

    xavier 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.