Welcome to the Linux Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Hi,
We are using Capture Driver on Netra DM8168 in field merge mode.
For the same settings of the driver and same input source, the driver's behaviour keeps changing (multiple runs produce different output) regarding which order the fields get merged in temporal sense (not spatial). The two variants are listed below
The questions we have are
Thansk and Regards,
Dileep Tamia
Dileep,
Reading field type is hw feature and not programmable. As the HW detects field, it informs the driver about field type. Top filed is always first . If top is followed by another top, it will be dropped. ( in driver terminology it is odd and even field)
Regards
Vimal
Vimal,
From your response I understand the following
Could you please confirm this.
Thanks and Regards,
Dileep