Welcome to the Linux Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Hello there,I am currently working with an embedded system based on a OMAP-L138.We are developing a Software Defined Radio (SDR) which is sending andrecieveing data in a slot-based scheme.Power management is a really important subject in our application,therefore we want to put the CPU into deepsleep (suspend to RAM) asmuch as we can.In short, this deepsleep-mode stops all the PLLs and put the SDRAMinto self-refresh.Since all the the PLLs is stopped in deepsleep-mode, we loose all timeperception. This is a problem since our rx/tx scheme is slot-based andif we don't know the time then we don't know when we shouldlisten/transmit.To solve this, we have implemented a timer in a FPGA that still tickswhen the CPU is sleeping. This timer also work as an alarm-clock, e.g.we can set a time when it should wake us up from deepsleep.When going into deepsleep, the driver that communicates with the FPGAset a wake-up alarm and then it calls pm_suspend(PM_SUSPEND_MEM).Our application is also time-critical so we want to go to/fromdeepsleep as fast as possible.For some quick measurements, we have seen that it takes about 70ms togo up from deepsleep.Now to the questions!1a.When we are going into deepsleep, all internal timers used by thekernel itself and other applications will be frozen and delayed. Doyou think this disorder will cause any problem?Of cause, this can be seen as a stupid question, it all depends on ourapplication, but if you have any personal experience about this, soplease feel free to mention how the reasoning went.1b.Should I take care of the internal timers (make the FPGA to wake upon those too)? Do you know any good functions that exposes a list withall timers?I guess there must be a function that gives you the timer that expiresnext but I have not found it.Is the timer_list and htimers handled the same way? I guess thehtimers is not jiffie-based?1c.Should I adjust some internal variables (e.g. jiffies) when waking up?2.Is it possible to speed up the time it takes to go to/from deepsleep?The pm_suspend() does a lot of things, eg. freeze processes, suspenddrivers and so on.Of cause, those functions is not there for fun, but is some moreimportant than others...?Thanks in advance