Hi,
I meet an Error while building the 8127 RDK project, it occurs at the label: #make mcfw_bios6. Below underline is the error info:
"/home/samba/IPNC/ti_tools/xdctools_3_22_04_46/packages/xdc/cfg/global.h", line 39: fatal error: could not open source file "/home/samba/1/ipnc_rdk/ipnc_mcfw/build/ipnc_rdk/obj/ti814x-evm/c6xdsp/release/ipnc_rdk_configuro/package/cfg/MAIN_APP_c6xdsp_pe674.h"
1 fatal error detected in the compilation of "/home/samba/IPNC/ipnc_rdk/ipnc_mcfw/build/ipnc_rdk/obj/ti814x-evm/c6xdsp/release/ipnc_rdk_configuro/package/cfg/MAIN_APP_c6xdsp_pe674.c".
Compilation terminated.
Above the red word '1' in the path should be 'IPNC', and it was defined an Micro xdc_cfg__header__ in global.h:
/* support old compiler option for naming config include file */
#ifdef xdc_cfg__header__
#define xdc_cfg__xheader__ <xdc_cfg__header__>
#endif
/* if specified, include configuration generated header */
#ifdef xdc_cfg__xheader__
#include xdc_cfg__xheader__
#endif
It seems automatically generated, so, how can I fix this problem ?
PS : The build platform is Ubuntu 10.04.4, RDK version is 2.0.0.
Thanks,
Pei Jacky.