i build dvsdk 4 from Ti ,but gets mang errors.i use 11.04 ubuntu to build it ,but the TI' doc say it must be built on ubuntu 10.04 .so Must I have to chang the host pc version ??.waiting your response,thank you
i am a talent
I think reason in other, e.g. I work in Debian GNU/Linux.
now the other question : i install dvsdk 4.1 to android source /extenal/ti-dsp. build ‘make TARGET_Product=omap3evm OMAPS=5.x -j2’ it ,but comes different errors.the errors all belong to dvsdk。
on other hand ,if i only build 'make' in the dvsdk ,it finally success.
so i have no ideas why ,
When you are building dvsdk for android, it uses the android toolchain and bionic libc etc, which is different from the standard ones.
You need to patch up the dvsdk to compile properly with android. Please look at the rowboat project page: http://code.google.com/p/rowboat/wiki/TI_DM37x_Android_2_3_4_MM_Acceleration
--------------------------------------------------------------------------------------------------------- Please click the Verify Answer button on this post if it answers your question.---------------------------------------------------------------------------------------------------------
---------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.---------------------------------------------------------------------------------------------------------