Hi,
I'm using AM335X-EVM board running Android ICS, I would like to get EVM's panel to run at 320x240 instead of 800x480.
I wrote at Android TI's forum and I've resolved part of the problems but at driver level other problems remain.
The panel I'm using is "TFC_S9700RTWV35TR_01B" and I can run it at the right resolution modifying $SOURCE_HOME/kernel/drivers/video/da8xx-fb.c at:
[2] = {
.name = "TFC_S9700RTWV35TR_01B",
.width = 800,
.height = 480,
.....
with
[2] = {
.name = "TFC_S9700RTWV35TR_01B",
.width = 320,
.height = 240,
.....
The problem I'm getting is the screen repeated on the short side of the screen, some vertical stripes and one horizontal in the middle.
I suppose I have to tweak the other parameters into da8xx-fb's driver but I don't know with which one I have to start. Do someone have some suggestions?
Thanks,
Francesco