This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ALSA driver

Guru 20420 points

Hello,

I would like to ask if it is possible to resample, i.e. downsample or upsample  in rx and tx direction.
What is the system call which does this resampling. I am using RDK linux, ALSA driver with DM8168,

Best Regards,

Ran

==========

  • Neither the hardware nor the kernel driver are capable of resampling.

    If your userspace accesses the device through alsa-lib, you can use its software resampler.

  • Guru 20420 points

    In reply to Clemens Ladisch:

    Hi Clemens,

    I see that the application uses API which are probably alsa-lib. I understand that I can now downsample or upsample using the library, though I did not yet find the API for that.

    Best Regards,

    Ran

    ==========

  • In reply to ranchu:

    Resampling is automatically enabled if you use a device name like "default" or "plughw". "hw" would bypass all alsa-lib enhancements.

  • Guru 20420 points

    In reply to Clemens Ladisch:

    Hi Clemens,

    Thank you very much for the answers.
    In my case device nsame is  "plughw" so I see that resampling is automatically enabled, but is there an API for changing the input rate or changing the playback sampling rate ?
    Can it be change to any value ?

    Best Regards,

    Ran

    ==========

  • In reply to ranchu:

    The "plughw" device behaves like a device that supports all sample rates.

    To change the input rate, just use another rate.

    The playback sample rate is the nearest rate actually supported by the hardware.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.