Hi everybody,
I’m following this guide in order to add CAN driver to my custom BSP:
http://processors.wiki.ti.com/index.php/AM335X_DCAN_Driver_Guide#CAN_Utilities
I’m using Ubuntu 10.04 LTS and the arago toolchain provided with SDK 05.06.00.00
I’ve exported all the needed variables but I'm having problems building libsocketcan:
After a successfully configuration and make (see log files)
I get this error:
marco@sheldon:~/temp/can/libsocketcan-0.0.8$ make install
Making install in include
make[1]: Entering directory `/home/marco/temp/can/libsocketcan-0.0.8/include'
make[2]: Entering directory `/home/marco/temp/can/libsocketcan-0.0.8/include'
make[2]: Nothing to be done for `install-exec-am'.
test -z "/home/marco/temp/can/libsocketcan-0.0.8/include" || /bin/mkdir -p "/home/marco/temp/can/libsocketcan-0.0.8/include"
/usr/bin/install -c -m 644 libsocketcan.h can_netlink.h '/home/marco/temp/can/libsocketcan-0.0.8/include/.'
/usr/bin/install: `libsocketcan.h' and `/home/marco/temp/can/libsocketcan-0.0.8/include/./libsocketcan.h' are the same file
/usr/bin/install: `can_netlink.h' and `/home/marco/temp/can/libsocketcan-0.0.8/include/./can_netlink.h' are the same file
make[2]: *** [install-nobase_includeHEADERS] Error 1
make[2]: Leaving directory `/home/marco/temp/can/libsocketcan-0.0.8/include'
make[1]: *** [install-am] Error 2
make[1]: Leaving directory `/home/marco/temp/can/libsocketcan-0.0.8/include'
make: *** [install-recursive] Error 1
marco@sheldon:~/temp/can/libsocketcan-0.0.8$
Where am I wrong?
Thanks!
Marco.