Hi all
I am using Appro DM368 IPNC 3.0 SDK, it works fine when I enabled only RTSP IE preview.
However, when I enable both the SD card recording and RTSP IE preview, the camera works well at the beginning, but after its continuous work at about 1 or 2 days, the video in SD card & IE preview becomes get paused and go on (which means the video looks like stops for a short while, and then skips to current frame)
I the UART output, we sam some following messages:
RET_OVERWRITE
RET_OVERWRITE
RET_OVERWRITE
Could you give some suggestions on this ?
BTW: the DDR size is 128MB, and 48MB for ARM Linux, 80MB for DSP encoder. And the Mem layout is following:
.profiles[VIDOE_INFO_MP4] =
{
.cache_size = 0xb00000,
.cache_blk_size = (100*1024),
.mem_size = 0x500000,
.mem_blk_size = (100*1024),
.ext_size = MP4_1_EXTRA_SIZE,
},