Hi all,
We are working on a product based on dm368 IPNC RDK 5.1. We have a requirement of using MMC1 to interface WiFi Module(WL1273) as SDIO interface
Wifi Module is working fine on MMC/SD1 when we configured pll's at a lower clock rates which is suggested for DM365. The Function clock for MMC/SD1 conntoller was 135 MHz and eventhough 135 MHz exceeds the maximum frequency limit of 100MHz(as specified in SPRUFH5B - MMC/SD controller userguide) module worked fine. But when we configured pll's for higher clock rate suggested for DM368, Wifi module is not working at all eventhough we tried function clock frequencies of 97MHz,106MHz,112MHZ,136MHz, and 170 MHz.
MMC/SD1 functional clock is generated from PLL1SYSCLK4 which itself is used for Config Bus, Peripheral System Interfaces, EDMA etc. So we have many constraints in adjusting the functional clock. Any suggestion to configure MMC/SD1 of DM368 are welcome
Please help on this. This is very urgent for us.