Hi,
I have setup the SDK and created the SD card by taking help from http://processors.wiki.ti.com/index.php/Sitara_Linux_SDK_create_SD_card_script
Everything that was expected was done as it is and response from the board was same as well (on booting none of the USER LED flashed).
But i'm not able to connect to my board while booting from SD Card. When I boot using Angstrom (provided with the board) I'm able to connect using minicom.
I'm using USBmini to USB cable to connect with my board.
As i wanna learn driver development using beaglebone black, i need kernel and complete source code in my board (which is not in Ansgtrom), hence using Angstrom isn't useful to me. please tell me how can i use SDK?
Also please let me know if SDK isn't made for device driver development as i'm not looking for application development for embedded linux.