I'm trying to program my uboot thru CCS. The GEL file I have is sticking at line 1408 in the DM814x_PG2.x.gel file I was using for the EVM.
//poll the status field to check if pll lock occured.
while ((RD_MEM_32(PCIE_PLLSTATUS) & 0x1 )!= 0x1);
Apparently the pll lock isn't happening. This is on our own board using the 8148. Is there a different gel file I should be using? Or is there a work around to this problem.
I tried commenting out that line, and I was able to go all the way through the flashing process...but it won't boot.
Help!
Dave