I enabled the TI DAVINCI RTC module in menuconfig of kernel of DM365. But the kernel loading process freezes as soon as RTC module is loaded. Here is the log:-
2) As evident, the loading is frozen at rtc's instance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I enabled the TI DAVINCI RTC module in menuconfig of kernel of DM365. But the kernel loading process freezes as soon as RTC module is loaded. Here is the log:-
Hi,
Are able to boot successfully if not enabled RTC in menuconfig or RTC pdata not passed in board file (i2c addr)?
Yes, i can successfully boot if the RTC is not enabled in menuconfig. Since I want to enable internal RTC, i did not try passing RTC pData in board file. Should I do this?
Hi,
Please refer our old e2e posts which is related to RTC fail cases like you,
http://e2e.ti.com/support/embedded/linux/f/354/t/84972.aspx
Try RTC driver as module driver (through menuconfig) after bootup linux (Ex: insmod rtc.ko)
Hi,
Since I receive the Reset RTC fail... from the UBL itself, don't u think it's possible that the bootloader is not initializing the rtc registers properly?
If that's a yes, then I think I should check the bootloader code? RSVP.