Hello everyone.
I'm working with a custom board based on am3352. The hardware design is similar to the beagle bone black. The linux distribution is obtained from the TI-SDK 7 arago kernel 3.12.10
I have a "simple" problem with the device tree to enable spi0 on / dev / spidev
During the phase of kernel settings from menuconfig , I enabled with [y] the following
Device Drivers ---> [*] SPI ---> <*> McSPI driver for OMAP
Device Drivers ---> [*] SPI ---> <*> User mode SPI device driver support
Then I modified the device tree as follows. The uart1 (dev/ttyO1)and the leds are working properly. I do not understand where the error might be with the spidev . Could you help me?
Any help is highly appreciated
The dts file modified is
am335x-bone-common.dtsi
/*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
/ {
model = "TI AM335x BeagleBone";
compatible = "ti,am335x-bone", "ti,am33xx";
cpus {
cpu@0 {
cpu0-supply = <&dcdc2_reg>;
};
};
memory {
device_type = "memory";
reg = <0x80000000 0x10000000>; /* 256 MB */
};
am33xx_pinmux: pinmux@44e10800 {
pinctrl-names = "default";
pinctrl-0 = <&clkout2_pin>;
user_leds_default: user_leds_default {
pinctrl-single,pins = <
0x28 (PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_a5.gpio1_21 gpmc_ad10.gpio_0_26 */
0x98 (PIN_OUTPUT_PULLUP | MUX_MODE7) /* gpmc_a6.gpio1_22 gpmc_wen.gpio_2_4 */
0x20 (PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_a7.gpio1_23 gpmc_ad8.gpio_0_22 */
0x40 (PIN_OUTPUT_PULLUP | MUX_MODE7) /* gpmc_a8.gpio1_24 gpmc_a0.gpio_1_16 */
>;
};
user_leds_sleep: user_leds_sleep {
pinctrl-single,pins = <
0x28 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_a5.gpio1_21 gpmc_ad10.gpio_0_26 */
0x98 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_a6.gpio1_22 gpmc_wen.gpio_2_4 */
0x20 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_a7.gpio1_23 gpmc_ad8.gpio_0_22 */
0x40 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_a8.gpio1_24 gpmc_a0.gpio_1_16 */
>;
};
i2c0_pins: pinmux_i2c0_pins {
pinctrl-single,pins = <
0x188 (PIN_INPUT_PULLUP | MUX_MODE0) /* i2c0_sda.i2c0_sda */
0x18c (PIN_INPUT_PULLUP | MUX_MODE0) /* i2c0_scl.i2c0_scl */
>;
};
uart0_pins: pinmux_uart0_pins {
pinctrl-single,pins = <
0x170 (PIN_INPUT_PULLUP | MUX_MODE0) /* uart0_rxd.uart0_rxd */
0x174 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart0_txd.uart0_txd */
>;
};
uart1_pins: pinmux_uart1_pins {
pinctrl-single,pins = <
0x180 (PIN_INPUT_PULLUP | MUX_MODE0) /* uart1_rxd.uart1_rxd */
0x184 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart1_txd.uart1_txd */
>;
};
mcspi0_pins: pinmux_mcspi0_pins {
pinctrl-single,pins = <
0x150 (PIN_OUTPUT_PULLUP | MUX_MODE0) /* spi0_sclk.spi0_sclk pagina 1117 spruh73j.pdf am335x trm*/
0x154 (PIN_INPUT_PULLUP | MUX_MODE0) /* spi0_d0.spi0_d0 */
0x158 (PIN_OUTPUT_PULLUP | MUX_MODE0) /* spi0_d1.spi0_d1 */
0x15C (PIN_OUTPUT_PULLUP | MUX_MODE0) /* spi0_cs0.spi0_cs0 */
>;
};
clkout2_pin: pinmux_clkout2_pin {
pinctrl-single,pins = <
0x1b4 (PIN_OUTPUT_PULLDOWN | MUX_MODE3) /* xdma_event_intr1.clkout2 */
>;
};
cpsw_default: cpsw_default {
pinctrl-single,pins = <
/* Slave 1 */
0x110 (PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxerr.mii1_rxerr */
0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mii1_txen.mii1_txen */
0x118 (PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxdv.mii1_rxdv */
0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mii1_txd3.mii1_txd3 */
0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mii1_txd2.mii1_txd2 */
0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mii1_txd1.mii1_txd1 */
0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mii1_txd0.mii1_txd0 */
0x12c (PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_txclk.mii1_txclk */
0x130 (PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxclk.mii1_rxclk */
0x134 (PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxd3.mii1_rxd3 */
0x138 (PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxd2.mii1_rxd2 */
0x13c (PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxd1.mii1_rxd1 */
0x140 (PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxd0.mii1_rxd0 */
>;
};
cpsw_sleep: cpsw_sleep {
pinctrl-single,pins = <
/* Slave 1 reset value */
0x110 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x114 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x118 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x11c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x120 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x124 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x128 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x12c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x130 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x134 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x138 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x13c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x140 (PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
davinci_mdio_default: davinci_mdio_default {
pinctrl-single,pins = <
/* MDIO */
0x148 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0) /* mdio_data.mdio_data */
0x14c (PIN_OUTPUT_PULLUP | MUX_MODE0) /* mdio_clk.mdio_clk */
>;
};
davinci_mdio_sleep: davinci_mdio_sleep {
pinctrl-single,pins = <
/* MDIO reset value */
0x148 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x14c (PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
mmc1_pins_default: pinmux_mmc1_pins {
pinctrl-single,pins = <
0x0F0 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat3.mmc0_dat3 */
0x0F4 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat2.mmc0_dat2 */
0x0F8 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat1.mmc0_dat1 */
0x0FC (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat0.mmc0_dat0 */
0x100 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_clk.mmc0_clk */
0x104 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_cmd.mmc0_cmd */
0x1A0 (PIN_INPUT_PULLUP | MUX_MODE7) /* mcasp0_aclkr.gpio3_18 */
0x160 (PIN_INPUT | MUX_MODE7) /* spi0_cs1.gpio0_6 */
>;
};
mmc1_pins_sleep: pinmux_mmc1_pins_sleep {
pinctrl-single,pins = <
0x0F0 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x0F4 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x0F8 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x0FC (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x100 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x104 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x1A0 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x160 (PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
emmc_pins: pinmux_emmc_pins {
pinctrl-single,pins = <
0x80 (PIN_INPUT_PULLUP | MUX_MODE2) /* gpmc_csn1.mmc1_clk */
0x84 (PIN_INPUT_PULLUP | MUX_MODE2) /* gpmc_csn2.mmc1_cmd */
0x00 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad0.mmc1_dat0 */
0x04 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad1.mmc1_dat1 */
0x08 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad2.mmc1_dat2 */
0x0c (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad3.mmc1_dat3 */
0x10 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad4.mmc1_dat4 */
0x14 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad5.mmc1_dat5 */
0x18 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad6.mmc1_dat6 */
0x1c (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad7.mmc1_dat7 */
>;
};
};
ocp {
uart0: serial@44e09000 {
pinctrl-names = "default";
pinctrl-0 = <&uart0_pins>;
status = "okay";
};
uart1: serial@48022000 {
pinctrl-names = "default";
pinctrl-0 = <&uart1_pins>;
status = "okay";
};
mcspi0: mcspi@48030000 {
compatible = "ti,omap2-mcspi";
#address-cells = <1>;
#size-cells = <0>;
ti,hwmods = "spi0";
ti,spi-num-cs = <4>;
pinctrl-names = "default";
pinctrl-0 = <&mcspi0_pins>;
status = "okay";
/*compatible = "ti,omap2-mcspi";
pinctrl-names = "default";
pinctrl-0 = <&spi0_pins>;
status = "okay";*/
};
musb: usb@47400000 {
status = "okay";
control@44e10000 {
status = "okay";
};
usb-phy@47401300 {
status = "okay";
};
usb-phy@47401b00 {
status = "okay";
};
usb@47401000 {
status = "okay";
};
usb@47401800 {
status = "okay";
dr_mode = "host";
};
dma-controller@07402000 {
status = "okay";
};
};
i2c0: i2c@44e0b000 {
pinctrl-names = "default";
pinctrl-0 = <&i2c0_pins>;
status = "okay";
clock-frequency = <400000>;
/* Set OPP50 (0.95V) for VDD core */
sleep-sequence = /bits/ 8 <
0x02 0x24 0x0b 0x6d /* Password unlock 1 */
0x02 0x24 0x10 0x02 /* Set DCDC3 to 0.95V */
0x02 0x24 0x0b 0x6d /* Password unlock 2 */
0x02 0x24 0x10 0x02 /* Set DCDC3 to 0.95V */
0x02 0x24 0x0b 0x6c /* Password unlock 1 */
0x02 0x24 0x11 0x86 /* Apply DCDC changes */
0x02 0x24 0x0b 0x6c /* Password unlock 2 */
0x02 0x24 0x11 0x86 /* Apply DCDC changes */
>;
/* Set OPP100 (1.10V) for VDD core */
wake-sequence = /bits/ 8 <
0x02 0x24 0x0b 0x6d /* Password unlock 1 */
0x02 0x24 0x10 0x08 /* Set DCDC3 to 1.1V */
0x02 0x24 0x0b 0x6d /* Password unlock 2 */
0x02 0x24 0x10 0x08 /* Set DCDC3 to 1.1V */
0x02 0x24 0x0b 0x6c /* Password unlock 1 */
0x02 0x24 0x11 0x86 /* Apply DCDC changes */
0x02 0x24 0x0b 0x6c /* Password unlock 2 */
0x02 0x24 0x11 0x86 /* Apply DCDC changes */
>;
tps: tps@24 {
reg = <0x24>;
};
};
};
leds {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&user_leds_default>;
pinctrl-1 = <&user_leds_sleep>;
compatible = "gpio-leds";
led@2 {
label = "beaglebone:green:heartbeat";
gpios = <&gpio0 26 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "heartbeat";
default-state = "off";
};
led@3 {
label = "beaglebone:green:mmc0";
gpios = <&gpio2 4 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "mmc0";
default-state = "off";
};
led@4 {
label = "beaglebone:green:usr2";
gpios = <&gpio0 22 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "cpu0";
default-state = "off";
};
led@5 {
label = "beaglebone:green:usr3";
gpios = <&gpio1 16 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "mmc1";
default-state = "off";
};
};
vmmcsd_fixed: fixedregulator@0 {
compatible = "regulator-fixed";
regulator-name = "vmmcsd_fixed";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
};
};
/include/ "tps65217.dtsi"
&tps {
regulators {
dcdc1_reg: regulator@0 {
regulator-always-on;
};
dcdc2_reg: regulator@1 {
/* VDD_MPU voltage limits 0.95V - 1.325V with +/-4% tolerance */
regulator-name = "vdd_mpu";
regulator-min-microvolt = <925000>;
regulator-max-microvolt = <1378000>;
regulator-boot-on;
regulator-always-on;
};
dcdc3_reg: regulator@2 {
/* VDD_CORE voltage limits 0.95V - 1.1V with +/-4% tolerance */
regulator-name = "vdd_core";
regulator-min-microvolt = <925000>;
regulator-max-microvolt = <1150000>;
regulator-boot-on;
regulator-always-on;
};
ldo1_reg: regulator@3 {
regulator-always-on;
};
ldo2_reg: regulator@4 {
regulator-always-on;
};
ldo3_reg: regulator@5 {
regulator-always-on;
};
ldo4_reg: regulator@6 {
regulator-always-on;
};
};
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <0>;
phy-mode = "mii";
};
&mac {
slaves = <1>;
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
};
&mmc1 {
status = "okay";
bus-width = <0x4>;
pinctrl-names = "default", "sleep";
pinctrl-0 = <&mmc1_pins_default>;
pinctrl-1 = <&mmc1_pins_sleep>;
cd-gpios = <&gpio0 6 GPIO_ACTIVE_HIGH>;
cd-inverted;
};
find /sys -name "*spi*"
/sys/bus/spi
/sys/bus/spi/drivers/spidev
/sys/bus/platform/devices/mcspi.3
/sys/bus/platform/devices/480ca000.spinlock
/sys/bus/platform/drivers/ti,dra7xxx-qspi
/sys/bus/platform/drivers/omap2_mcspi
/sys/devices/ocp.2/mcspi.3
/sys/devices/ocp.2/480ca000.spinlock
/sys/class/spi_master
/sys/class/spidev
/sys/module/regmap_spi
/sys/module/spidev
Marco