Hi,
I want to boot AM335x EVM with usb booting,
I have created SD card with command
"sudo ./create-sdcard.sh"
and installed default MLO, uboot.img, zImage and rootfs from SDK 7.0 later I placed the SD card and booted up to u-boot, then removed sd card and connected to USB port through adapoor and followed the commands,
U-Boot # usb start U-Boot # setenv mmcroot /dev/sda2 ro U-Boot # run mmcargs U-Boot # run bootcmd_usb
linux booted sucessfully but the porblem is it stuck at mounting file system as
2.289551] Detected MACID = 00:18:31:8f:57:fe
[ 2.296714] input: volume_keys.8 as /devices/volume_keys.8/input/input2
[ 2.304642] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801)
[ 2.317598] Waiting for root device /dev/sda2...
[ 60.321387] PM: request_firmware failed
Can any one please let me know where its going wrong.