You know keystone 2 series multicore SOIC contains 4 ARM cores and we can use them with SMP linux kernel. I can disable SMP support from kconfig and change the device tree structure for each kernel . But exactly I did not find any example that show how to boot multiple linux kernels from single u-boot. Also for multicore only one arm core is the master at first. This master core enables the other cores to run.
I think u-boot must do some extra stuff on the master core and load all kernel+filesystem and DTS to the memory for other linux instances and run them. Is it possible to do this ?