Dear Forum,
I am trying to establish a "well known" state of the SDK 7.0 before doing any changes.
- I have run the setup.sh with all (except /dev/ttyUSB0) default choises.
- The /tftpboot and ../targetNFS dirctories are initialized as default.
- I let the setup modify the BBB target uEnv.txt (later modified to fixed ip, no dhcp due to gateway)
- The Rules.make file content seem correct with am335x-evm and armv7-a settings.
- I run the "make u-boot-spl" without errors.
- I run "make clean", "make all", "make install" without any errors.
- I notice that the timestamp in the /tftpboot directory have not changed.
Questions:
- Why are the files in the "tftp root" directory not updated when running make?
- Why are not the u-boot files placed/copied into the /tftpboot when running "make u-boot-spl"?
- How/where is initrd.img for the RAM image generated (have copied an old one)?
Please advice
Best regards
Terje Froysa