Hi,
I'm trying to use netconsole in linux.
I've compiled the linux clean with CONFIG_NETCONSOLE & CONFIG_NETCONSOLE_DYNAMIC:
-dvr-rdk$ cat .config | grep "NETC"
CONFIG_NETCONSOLE=y
CONFIG_NETCONSOLE_DYNAMIC=y
I first tried to boot linux with netconsole. I then got message "console [tty0] enabled, bootconsole disabled" for some seconds, but it continue the printing to console as following:
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
console [tty0] enabled, bootconsole disabled
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm814x ttyO0
Arago 2012.10 dm814x ttyO0
dm814x login: root
root@dm814x:~# cd /sys/
I also tried to set the netconsole dynamic, the netconsole folder is missing in
cd /sys/kernel/config/ , i.e. I dont have /sys/kernel/config/netconsole/
All the netconsole is issue is relevant because I'm still trying to use KGDB. If there is some solution to my problem of using kgsb, It will be helpful
http://e2e.ti.com/support/embedded/linux/f/354/p/358670/1260155.aspx#1260155
Thanks,
Ran