Hi,
I want to use the DCAN interface on PRU-ICSS to send/receive data present on DDR RAM at a fixed physical address.
- Address of DDR is 0x8000_0000 to 0x9000_0000(256MiB)
- My buffer is present at 0x8FF0_0000 to 0x9000_0000 (1MiB)
As soon as I access the hardware address 0x8FF0_0000 the PRU-ICSS goes into some faulty state and becomes unresponsive.
Is there some other way to access DDR from PRU-ICSS ?
Rakesh