In order to avoid conflicts in the use of peripherals for a DSP audio application for the OMAP-L137 EVM, I have disabled the audio and I2C drivers as per the instructions here. Unfortunately a side effect of this is that I no longer have Ethernet connectivity. When booting, I get the following error:
MAC address is deadbeaf
...
Setting up networking ....
/etc/network/options is deprecated.
Setting up IP spoofing protection: rp_filter done.
Disabling IPv4 packet forwarding: done.
Disabling TCP/IP Explicit Congestion Notification: done.
Starting network interfaces: Error, dhcpStart: ioctl SIOCGIFHWADDR: No such device
Failed to bring up eth1.
I have not had a lot of time to look into this issue, however it would be very helpful if we could still have Ethernet on the board. Looking at the schematics for the board, there seems to be some MUXing between the Ethernet and McASP pins which might explain the problem. Also I'm not sure if I2C is used to communicate with other chips used for Ethernet.
Can someone please advise on how to have Ethernet enabled without audio/I2C, and/or if it is even possible.