obviously, this becomes a "path not found" error when I try to compile later the package!
I am trying to build and install gst-plugins-bad unto Sitara SDK v7.0.
The SDK had gstreamer-0.10 and gst-plugin-bad old versions preinstall into it.
Since I wanted to install on of the latest gst-plugins-bad (v1.4.0), I found from reading discussion forums that I needed latest gstreamer-1.x as gstreamer base to be able to install latest gst-plugins.
I went on and installed latest gstreamer (v1.4.0) unto this Sitara SDK v7.
So now, I have both versions into my SDK: gstreamer-0.10 and gstreamer-1.4.0.
I tested the newly install gstreamer-1.4.0 (gst-launch-1.0) and it works well on my Sitara board.
Now I try to configure my environment to build and install gst-plugins-bad-1.4.0:
I followed instructions from section "Configure/Autotools" from "Sitara Linux SDK GCC Toolchain" TI web page (http://processors.wiki.ti.com/index.php/Sitara_Linux_SDK_GCC_Toolchain#Usage).
Unfortunately, when I run following command to configure my host system (from gst-plugin-bad-1.4.0 folder installed in my Ubuntu) , I am getting an un-logical error about gstreamer version mismatch!!!!!!
//////////////////////////////////////////////////////////////////////////////////////////////////////////
$ ./configure --host=i686 --disable-deinterlace2 --disable-x264
.....
....
checking for glib-mkenums... glib-mkenums
checking for GIO... yes
checking for GST... no
configure: No package 'gstreamer-1.0' found
configure: error: no gstreamer-1.0 >= 1.4.0 (GStreamer) found
//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
I already have gstreamer-1.4.0 installed in the SDK and it run fine on my Sitara target, so I do not understand the meaning of this error!!!!
Is TI ever came across this kind of issue when integrating gstreamer and its plugins into their Sitara SDKs?