Hi Experts,
I had downloaded and installed the Linux SDK package 7.0 for beagle bone board.
I tried to compile the linux sources inside the folder /xx/sdk-7.0/board_packages/linux-3.12/ after copying the ti-sdk-am335x config file it compiles successfully. But when I disable particular driver in the default configuration file using make menuconfig and then I tried to re-compile it. This time it is showing an error message as follows
warning : (SOC_OMAP5 && SOCDRA7xx) selects ARM_xxxx which has unmet direct dependencies
Restart Config..
Then it is prompting to select whatever the settings left out. Why it occurs ?
Where the SDK is getting reference for the default board package (some folder inside the SDK folder structure) ?
Regards,
Lyf