Hello,
I'm doing boot on UART , I already done that in the past with success, but now it acts differently
I would like to ask what is the meaning of "Reset button" below. When I reset the board I get "CC.." again.
I will appreciate your fast response,
Boot Over UART
Note
The release package does not contain the binary for UART boot. Please follow the steps mentioned
#U-Boot_UART_support for UART boot for compiling u-boot.min.uart
1. Switch ON EVM with switch settings for UART boot. When “CCCC” characters appear on TeraTerm window,
from the File Menu select Transfer --> XMODEM --> Send (1K mode)
2. Select “u-boot.min.uart” for the transfer
3. Press "Reset button" to initiate image download
4. After image is successfully downloaded, the ROM code will boot it.
5. Hit enter and get to u-boot prompt “TI-MIN#
Thanks,
Ran