Hi Experts,
I would like to disable the entire hardware module from the linux kernel.
Say I am not using the SPI interface is it possible to disable all interrupts and programs related to the SPI interface ?
Is it achieved through the simple "make menuconfig" or have to do it further down inside the kernel ?
The prime objective is to disable all the events and interrupts related to that module.