Hi guys,
Can you please give me the git hash ref of the Linux Keystone Kernel source that was used to generate the kernel and dtb images for MCSDK 3.00.03.15 for the hawking EVM.
Nitish
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi guys,
Can you please give me the git hash ref of the Linux Keystone Kernel source that was used to generate the kernel and dtb images for MCSDK 3.00.03.15 for the hawking EVM.
Nitish
Hi Nitish,
You can do git update or git pull for the latest releases and do "git" command for TAG listing then you can do a "git reset" to the particular mentioned version.
http://processors.wiki.ti.com/index.php/MCSDK_UG_Chapter_Exploring#Changes_impacting_users
Hi Stalin,
Thank you for your response.
DEV.MCSDK-{version} do not seem to exist in the http://git.ti.com/keystone-linux/linux repository. Is there another repository I should be looking at? The only tags here are the mainline linux kernel release tags v3.10, v3.11 etc, and then some tags that TI have put in that begin K2_RT_LINUX_{version}. But no tag that looks like it could be related to MCSDK 3.00.03.15. Is it possible these tags were removed?
Nitish
You should be referring first the release note for the MCSDK release which is available as part of the release. This has a table of the components and the tag. You will find the kernel tag from this table. Then do a git reset --hard to the tag and it will point the kernel code to the released version.