Hi There,
I am using DRA7xx platform (Jacinto 6) for automotive application enablement.
We are using the IPU2 for early video decode and we observed strange timing behaviour in IPU2 firmware loading.
Version - GLSDK 6.04.00.02 and corresponding IPC version is ipc_3_21_00_07.
Actual issue -
dra7-ipu2-fw.xem loading and rpmsg-dce message arrival takes ~ 650 ms. Is that fixed or we have some opportunity to optimize it? We are not using the late attach feature as that is not an option for us.
It seems most of the time is spent in M4 Startup till it lands at M4 side main function. Does it have to do with several static module loading or SYS/BIOS initialization time?
Any help would be great to reduce this load and trigger time.
Thanks & Regards,
-Harshit