Hi,
im trying to config an LCD driver for DM3730 in ../arch/arm/mach-omap2/board-omap3logic.c
do i need to config an spi_board_info and set its parameters or can i just create a new driver in a new file using just spi_device instead?
*the driver has to be a module with init and exit functions so im not sure if its even possible to configure it via board-omap3logic.c...:/
Thanks!