I've been searching around trying to find the best way to do video streaming on an 814x using Graphics SDK. I have Linux 04_04_00_02 and Graphics SDK 4_06_00_03. I've followed the wiki Graphics SDK Quick installation and user guide and the OpenGL applications run fine on the target. I've also installed qt version 4.8.6 following the Building Qt with OpenGL ES accelerated by SGX and can run the demos fine. Now I would like to do video streaming, either with OpenGL ES with accelerated SGX or with Qt wrapped around but I am not sure of the correct approach. I have seen terms like bufferclass, eglimage, and v3dfx. Which of this would be recommended to use on the TI814x embedded platform for video streaming?
By the way, I have tried v3dfx applications using Qt and OpenGL but I didn't have much luck getting that to work. I ran the qt-v3dfx-base-test application and get a Segmentation fault. I didn't want to spend too much time trying to figure it out because I didn't know if v3dfx is even supported....or had been tested on an 814x.
If you could just point me in the correct approach (bufferclass, eglimage, and/or v3dfx) for video streaming on an 814x that would be great.
Thanks,
Kim