Hi,
I am new to the embedded linux environment. Please help in solving the following issue.
I am working on am335x_evm and ti-sdk-am335x-evm-07.00.00.00-Linux-x86-Install. When I am trying to create sd card images using the script only MLO and u-boot.img are being copied into boot partition. And the board is being stopped at Uboot as there is no kernal image. The log while creating the sd card image is as follows. Even with sdk version 06.00 the same problem is existing. My requirement is now I have to edit the dts file for other serial ports enabling(other than console) and compile the kernel and use the serial port from user interface application. Even Im copying the uImage, dtb files manually its not working. And I have doubts on uEnv.txt file also. Uboot is searching for this file if its not existing then stops booting kernel. I tried to keep a file just the name uEnv.txt then the uImage is being copied but stopped at Starting kernal..... log. Pleas hlep me in solving these issues. Please give details for each query. Thanks in anticipation.
Log for sd card script:
Device Boot Start End #cyls #blocks Id System
/dev/sdb1 * 0+ 8 9- 72261 c W95 FAT32 (LBA)
/dev/sdb2 10 239 230 1847475 83 Linux
/dev/sdb3 0 - 0 0 0 Empty
/dev/sdb4 0 - 0 0 0 Empty
Successfully wrote the new partition table
Re-reading the partition table ...
If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
################################################################################
Partitioning Boot
################################################################################
mkfs.vfat 3.0.12 (29 Oct 2011)
################################################################################
Partitioning rootfs
################################################################################
mke2fs 1.42 (29-Nov-2011)
Filesystem label=rootfs
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
115680 inodes, 461868 blocks
23093 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=473956352
15 block groups
32768 blocks per group, 32768 fragments per group
7712 inodes per group
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912
Allocating group tables: done
Writing inode tables: done
Creating journal (8192 blocks): done
Writing superblocks and filesystem accounting information: done
################################################################################
Partitioning is now done
Continue to install filesystem or select 'n' to safe exit
**Warning** Continuing will erase files any files in the partitions
################################################################################
Would you like to continue? [y/n] : y
Mount the partitions
Emptying partitions
Syncing....
################################################################################
Choose file path to install from
1 ) Install pre-built images from SDK
2 ) Enter in custom boot and rootfs file paths
################################################################################
Choose now [1/2] : 1
Will now install from SDK pre-built images
now installing: ti-sdk-am335x-evm-07.00.00.00
################################################################################
Copying files now... will take minutes
################################################################################
Copying boot partition
MLO copied
u-boot.img copied
Copying rootfs System partition
Written 100%
Syncing...
Un-mount the partitions
Remove created temp directories
Operation Finished
Regards,
Vijaykumar Ponugoti