Since i am new to the linux environment , I need some linux evaluation board for Automation setup(Iot) could you ppl please provide me a solution on this . i have pasted the requirement here.
I am expecting
- Ease of Use
- This must be guiding point as expectation is anyone with knowledge of python can add test cases
- Availability of GPIO's, USB(4-5 Nos), CAN, Ethernet, UART(3-4 Nos) , PWM, ADC, DAC, I2C, SPI etc
- Voltage Comparability of peripherals .(1.8 to 3.3V)
- Standard OS (linux)
- Availability of drivers to Access Peripherals(GPIO, SPI, I2C ...) with python script
- Community Support
- Easily Integrated in our set-up
Ex : Board like Raspberry Pi, BeagleBone black.