Hello,
I would like to ask if there is some simple way to turn the ethernet power off/on (for power save), if yes - how ?
Also We need that while the ethernet is off to enable wakeup in case that ethernet packets are recieved .
I am using OMAP3530 with psp 4.2.0.7, with SMSC911x phy. It seems that smsc911 support WOL (wake on lan).
Is it simply done by using ethtool or do I need to configure the linux to support WOL
?
Regards,
Ran