Hi,
I have questions about TI Sitara SDK.
Please tell me if someone have information.
Q1: Demo application of current SDK is implemented with Qt4,
Is Qt5 supported in the future?
Q2: I think that Arago project Linux is using QWS windows system insted of X11, but Qt5 is not possible to use the QWS.
If Qt5 is supported, what window system is used?
Q3: If Qt5 is not supported, is UI framework other than Qt scheduled?
Best regards,
H.U