Hello all!
I have a custom board on TI C6678. I have latest clone linux-c6x running on core 0. On board placed 2GB of DDR3 RAM, but I can't change memory size via command line more than exist by default: 256MB. If I try to use 128MB or 192MB - size is changing (cat /proc/meminfo).
Please. tell me how I can pass correct command line parameters for kernel?
Here is example of my command line (from product folder):
./bootblob set-cmdline xxx.bin 'console=ttyS0,115200 earlyprintk \
ip=192.168.0.249:::255.255.254.0:target:eth0:off \
mem=512M@0x80000000'
May be I need change kernel source code, in addition to command line arguments?
Thank you.