Hi,
I have installed glsdk 7.00 and while following the instructions given in GLSDK User guide I have got the following problem. Plz help me.
After giving the executing ./build-core-sdk.sh dra7xx-evm on my host PC, there were several logs, warnings and it took several minutes. At the end i got following error.
ERROR: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/home/medha/ti-glsdk_dra7xx-evm_7_00_00_04/yocto-layers/downloads/git2/gitorious.org.matrix-gui-v2.matrix-gui-v2-apps.git'...
fatal: The remote end hung up unexpectedly
ERROR: Function failed: Fetcher failure for URL: 'git://gitorious.org/matrix-gui-v2/matrix-gui-v2-apps.git;protocol=git;branch=master'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/medha/ti-glsdk_dra7xx-evm_7_00_00_04/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/all-oe-linux/matrix-gui-apps-images/2.0-r27.0/temp/log.do_fetch.15262
ERROR: Task 3403 (/home/medha/ti-glsdk_dra7xx-evm_7_00_00_04/yocto-layers/sources/meta-arago/meta-arago-extras/recipes-core/matrix/matrix-gui-apps-images_2.0.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1623 tasks of which 0 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:
Summary: 1 task failed:
/home/medha/ti-glsdk_dra7xx-evm_7_00_00_04/yocto-layers/sources/meta-arago/meta-arago-extras/recipes-core/matrix/matrix-gui-apps-images_2.0.bb, do_fetch
Summary: There were 103 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
[GLSDK]>
[GLSDK]> Completed Yocto build at Wed Apr 1 14:35:57 IST 2015
[GLSDK]>
What is the issue.? Will it cause any problem further.?
Thanks and Rgds,
Vijay