Hi,
I boot Linux on my EVMK2H, and then attempt, using CCSv6 through XDS200, to run a simple app. such as helloworld, on any of the DSP cores.
I get the following message: Error connecting to the target: (Error -1180 @ 0x0). Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.1.641.0)
I have checked the cores using mpmcl and they are OK, and I can run compiled code on them.
I have also tried setting the Linux environmental variable debug_options to 1, to no avail. Also have reduced XDS clock speed. All is Vanity futility.
Help. How do I take the core (?) out of reset?
Thanks,
Bernard