I am trying to partition eMMC of BBB(am335x) based custom board, I am using sfdisk to do that. I am using following command to do that,
#Partition emmc sfdisk -D -H 255 -S 63 -C 467 /dev/mmcblk0 -uM << EOF ,32,C,* ,200,L ,200,L ,,E ,100,L ,60,L ,200,L ;1269,L ; EOF
But sfdisk shows following partitions and
# fdisk -l /dev/mmcblk0 Disk /dev/mmcblk0: 3841 MB, 3841982464 bytes 255 heads, 63 sectors/track, 467 cylinders Units = cylinders of 16065 * 512 = 8225280 bytes Device Boot Start End Blocks Id System /dev/mmcblk0p1 * 1 5 40131 c Win95 FAT32 (LBA) /dev/mmcblk0p2 6 31 208845 83 Linux /dev/mmcblk0p3 32 57 208845 83 Linux /dev/mmcblk0p4 58 467 3293325 5 Extended /dev/mmcblk0p5 58 70 104391 83 Linux /dev/mmcblk0p6 71 78 64228+ 83 Linux /dev/mmcblk0p7 79 104 208813+ 83 Linux /dev/mmcblk0p8 105 266 1301233+ 83 Linux /dev/mmcblk0p9 267 467 1614501 83 Linux
but I don't see /dev/mmcblk0p8 and /dev/mmcblk0p9. Because of that i am not able to format the /dev/mmcblk0p8. Can anyone suggest what could be the problem ?
is there a limit on creating extended partitions ?