Hi Team,
am using unjiflash software for flashing my beagle bone black board.
i configure ip address and located all image files in folder but problem is flash the image still progress will be 0%
Network ip : 192.168.2.1
IP Lease : 600
DHCP IP Rane Low : 192.168.2.2
DHCP IP Rane High : 192.168.2.254
TFTP Server Ip :192.168.2.1
TFTP Home folder : C:\AM335x_Flashtool\images
This folder contains - MLO , u-boot.img , uImage ,am335x-boneblack.dtb,rootfs,debricks.txt.
Control port :3347
Device Mac Address : d0;39:72:3b:89:40
Ip addr : 192.168.2.2
status : Flash progress
Progress % : 0
but problem is flashing always shows 0% but i did not understand problem
Regards,
Naveen,