Hi,
Going exactly by the instructions at
http://processors.wiki.ti.com/index.php/MCSDK_UG_Chapter_Exploring#Yocto8561.config.log
with all exports done as outlined and with Linaro Toolchain installed like
http://arago-project.org/wiki/index.php/Setting_Up_Build_Environment
The build is running for a while (about 750 tasks of 6300) and then I am getting the following error
| configure: exit 1
| ERROR: oe_runconf failed
| ERROR: Function failed: do_configure (see /home/gunter/oe/mcsdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/classpath-native/0.99-r6.0/temp/log.do_configure.22224 for further information)
ERROR: Task 4780 (/home/gunter/oe/mcsdk/oe-layersetup/sources/meta-java/recipes-core/classpath/classpath-native_0.99.bb, do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 748 tasks of which 740 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:
Summary: 1 task failed:
/home/gunter/oe/mcsdk/oe-layersetup/sources/meta-java/recipes-core/classpath/classpath-native_0.99.bb, do_configure
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
Digging deeper I am looking at the config.log file at
/home/gunter/oe/mcsdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/classpath-native/0.99-r6.0/classpath-0.99/config.log
it is attached. Here I find that a bunch of include files are missing, e.g.
gunter@gunter-Latitude-E4300:~/oe/mcsdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/classpath-native/0.99-r6.0/classpath-0.99$ grep fatal config.log
conftest.c:11: fatal error: ac_nonexistent.h: No such file or directory
conftest.cpp:24: fatal error: ac_nonexistent.h: No such file or directory
conftest.cpp:24: fatal error: ac_nonexistent.h: No such file or directory
conftest.c:24: fatal error: ac_nonexistent.h: No such file or directory
conftest.c:64: fatal error: sys/config.h: No such file or directory
conftest.c:31: fatal error: sys/config.h: No such file or directory
conftest.c:69: fatal error: sys/utime.h: No such file or directory
conftest.c:36: fatal error: sys/utime.h: No such file or directory
conftest.c:69: fatal error: sys/filio.h: No such file or directory
conftest.c:36: fatal error: sys/filio.h: No such file or directory
conftest.c:71: fatal error: crt_externs.h: No such file or directory
conftest.c:38: fatal error: crt_externs.h: No such file or directory
conftest.c:74: fatal error: sys/event.h: No such file or directory
conftest.c:41: fatal error: sys/event.h: No such file or directory
conftest.c:79: fatal error: sys/loadavg.h: No such file or directory
conftest.c:46: fatal error: sys/loadavg.h: No such file or directory
conftest.c:79: fatal error: sys/sockio.h: No such file or directory
conftest.c:46: fatal error: sys/sockio.h: No such file or directory
conftest.c:49: fatal error: sys/config.h: No such file or directory
conftest.c:146: fatal error: gmp.h: No such file or directory
conftest.c:113: fatal error: gmp.h: No such file or directory
BTW, build-essentials are installed, not sure where the include files should be coming from, whether there is an include path missing ...
Please let me know.
Thanks,
--Gunter