Dear All
I have pair ARM1 & DSP file, binary files , that are connected through DSP link.
Then i create a new ARM codes, and adjust the memory pool to load the DSP binary to be the same as the DSP binary, the new ARM is ARM2.
When i run the ARM2, it loads the DSP binary successfully, but only the main.cpp file in the DSP being running, while the rest of the files, are not executed.
meanwhile, if i coubple the ARM1 and DSP, the whole DSP .cpp files are being executed.
Could anyone help, me what should i fix.
Regards
Ibrahim B