Hey,
I've just started developing C6678 DSP board, which has a Linux on it. I'm now trying to run a helloworld program on the onboard linux. Here is what I did:
I build a helloworld program in CCS, and use the debug mode to load and run the application (helloworld.out) through XDS560 emulator, and it works well.
Then I use ftp to transfer the helloworld.out file to the DSP board, and try to run it there (./helloworld.out ), and the SEGV pops out.
I'm guessing maybe this is not the right way to get an application running on the onboard Linux?
Thanks in advance,
Shang