Hi,
I'm loading a 16bit bootlogo.bmp on system boot but the colors are all wrong,
the LCD is 24bit and on boot it works on 16bit mode cause i cant get it to work on 24bit.(when the kernel loads i reconfigure it to 24bit and everything works fine).
If set to 24bit with 24bit bootlogo then nothing is displayed.
the board is DM3730.
any help is appreciated.
,thanks.