Hello
I was trying to build Linux Kernel FOR K2H EVM. I was following the MCSDK User Guide . In the 3.3.5 Build procedure, I type "MACHINE=k2hk-evm TOOLCHAIN_BRAND=linaro ARAGO_BRAND=mcsdk bitbake tisdk-server-rootfs-image". And then I got the following errors (part of terminal output is showing).
Can anyone help me with that? I am using Ubuntu-14.04.
Thanks.
Xining Yu
make[3]: Leaving directory `/home/iart/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/bfd/po'
| make[3]: Entering directory `/home/iart/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/bfd/po'
| make[3]: Nothing to be done for `info'.
| make[3]: Leaving directory `/home/iart/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/bfd/po'
| make[3]: Entering directory `/home/iart/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/bfd'
| make[3]: Nothing to be done for `info-am'.
| make[3]: Leaving directory `/home/iart/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/bfd'
| make[2]: *** [info-recursive] Error 1
| make[2]: Leaving directory `/home/iart/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux/bfd'
| make[1]: *** [all-bfd] Error 2
| make[1]: Leaving directory `/home/iart/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/binutils-2.20.1/build.x86_64-linux.x86_64-linux'
| make: *** [all] Error 2
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (see /home/iart/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/2.20.1-r9/temp/log.do_compile.31639 for further information)
ERROR: Task 714 (virtual:native:/home/iart/oe-layersetup/sources/meta-arago/meta-arago-extras/recipes-devtools/binutils/binutils_2.20.1.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 348 tasks of which 72 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:
Summary: 1 task failed:
virtual:native:/home/iart/oe-layersetup/sources/meta-arago/meta-arago-extras/recipes-devtools/binutils/binutils_2.20.1.bb, do_compile
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.