Hii,
We have developed our customized board with AM5728 processor and while booting from memory card on the console i am getting the below messages and stops. What can be the reason?
OMAP SD/MMC: 0<CR><LF>
reading u-boot.img<CR><LF>
reading u-boot.img<CR><LF>
<CR><LF>
<CR><LF>
U-Boot 2013.04 (Jun 25 2015 - 19:30:24)<CR><LF>
<CR><LF>
CPU : DRA752 ES1.1<CR><LF>
Board: DRA7xx<CR><LF>
I2C: ready<CR><LF>
DRAM: 1.5 GiB<CR><LF>
WARNING: Caches not enabled<CR><LF>
MMOMAP SD/MMC: 0, OMAP SD/MMC: 1<CR><LF>
Using default environment<CR><LF>
<CR><LF>
The same u-boot code is working fine with EVM. After debugging u-boot code i have found that after printing puts("Using default environment\n\n");
it hangs in the function
himport_r(&env_htab, (char *)default_environment, sizeof(default_environment), '\0', flags, 0, NULL).
||
hsearch_r(e, ENTER, &rv, htab, flag)
||
env_flags_init(&htab->table[idx].entry); ------------------ Hangs here, in this function
What can be the possible reasons and soluions?
Thanks & Regards,
Ganesh