Dear Support,
I am trying to port the AIC32x4 driver on the AM335x SoC. The driver is already available and I followed the TI Wiki to port the codec driver.
I would ask what are exactly the steps to have the audio card registered, since the "ALSA device list" is always "no soundcard found".
During the boot the audio codec is registered and the mcasp too.
Oddly, in the snd_soc_card, I had to increase the .num_links since with a value of 1 the boot crashed in thesoc-core.c in the snd_soc_register_dais function, here:
list_add(&dai->list, &dai_list);
Below the dmesg I had, I put some extra printk to debug.
Thank you in advance.
[ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 3.14.26-gb9df364-dirty (ermes@linux-ermes) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #31 Wed Jul 22 14:59:22 CEST 2015 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine model: TI AM335x Ermes ST452 [ 0.000000] cma: CMA: reserved 24 MiB at 8c800000 [ 0.000000] Memory policy: Data cache writeback [ 0.000000] On node 0 totalpages: 65024 [ 0.000000] free_area_init_node: node 0, pgdat c0868cf4, node_mem_map cfbee000 [ 0.000000] Normal zone: 512 pages used for memmap [ 0.000000] Normal zone: 0 pages reserved [ 0.000000] Normal zone: 65024 pages, LIFO batch:15 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (neon ) [ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768 [ 0.000000] pcpu-alloc: [0] 0 [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64512 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/nfs nfsroot=192.168.0.229:/home/ermes/ti-processor-sdk-linux-am335x-evm-01.00.00.00/targetNFS,nolock rw ip=dhcp [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Memory: 224236K/260096K available (5851K kernel code, 321K rwdata, 2132K rodata, 269K init, 232K bss, 35860K reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc07d4054 (7985 kB) [ 0.000000] .init : 0xc07d5000 - 0xc08185e4 ( 270 kB) [ 0.000000] .data : 0xc081a000 - 0xc086a760 ( 322 kB) [ 0.000000] .bss : 0xc086a760 - 0xc08a4778 ( 233 kB) [ 0.000000] NR_IRQS:16 nr_irqs:16 16 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000030] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956969942ns [ 0.000077] OMAP clocksource: timer1 at 24000000 Hz [ 0.000673] Console: colour dummy device 80x30 [ 0.000734] Calibrating delay loop... 298.59 BogoMIPS (lpj=1492992) [ 0.068495] pid_max: default: 32768 minimum: 301 [ 0.068727] Security Framework initialized [ 0.068847] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.068876] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.085953] CPU: Testing write buffer coherency: ok [ 0.086693] Setting up static identity map for 0x805bc560 - 0x805bc5b8 [ 0.088853] devtmpfs: initialized [ 0.093366] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.111493] omap_hwmod: tptc0 using broken dt data from edma [ 0.111703] omap_hwmod: tptc1 using broken dt data from edma [ 0.111891] omap_hwmod: tptc2 using broken dt data from edma [ 0.118282] omap_hwmod: debugss: _wait_target_disable failed [ 0.188317] pinctrl core: initialized pinctrl subsystem [ 0.190695] regulator-dummy: no parameters [ 0.195440] NET: Registered protocol family 16 [ 0.200435] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.206543] cpuidle: using governor ladder [ 0.206583] cpuidle: using governor menu [ 0.223694] syscon 44e10000.control_module: regmap [mem 0x44e10000-0x44e107fb] registered [ 0.227282] platform 49000000.edma: alias fck already exists [ 0.227341] platform 49000000.edma: alias fck already exists [ 0.227380] platform 49000000.edma: alias fck already exists [ 0.229470] gpiochip_add: registered GPIOs 0 to 31 on device: gpio [ 0.230187] OMAP GPIO hardware version 0.1 [ 0.232117] gpiochip_add: registered GPIOs 32 to 63 on device: gpio [ 0.234528] gpiochip_add: registered GPIOs 64 to 95 on device: gpio [ 0.236952] gpiochip_add: registered GPIOs 96 to 127 on device: gpio [ 0.264843] No ATAGs? [ 0.264890] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.331830] bio: create slab <bio-0> at 0 [ 0.370533] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver [ 0.372154] of_get_named_gpiod_flags: can't parse gpios property of node '/fixedregulator@0[0]' [ 0.372824] vbat: 5000 mV [ 0.373111] of_get_named_gpiod_flags: can't parse gpios property of node '/fixedregulator@1[0]' [ 0.373739] vmmcsd_fixed: 3300 mV [ 0.374108] of_get_named_gpiod_flags exited with status 0 [ 0.374896] vtt: 1500 mV [ 0.382728] vgaarb: loaded [ 0.383999] i2c-core: driver [palmas] using legacy suspend method [ 0.384027] i2c-core: driver [palmas] using legacy resume method [ 0.385749] SCSI subsystem initialized [ 0.387003] libata version 3.00 loaded. [ 0.389489] usbcore: registered new interface driver usbfs [ 0.389969] usbcore: registered new interface driver hub [ 0.390459] usbcore: registered new device driver usb [ 0.392759] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c0_pins, deferring probe [ 0.392826] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral [ 0.392897] omap_i2c 4802a000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c1_pins, deferring probe [ 0.392934] platform 4802a000.i2c: Driver omap_i2c requests probe deferral [ 0.393874] pps_core: LinuxPPS API ver. 1 registered [ 0.393902] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.394235] PTP clock support registered [ 0.399110] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.401218] Advanced Linux Sound Architecture Driver Initialized. [ 0.404953] Switched to clocksource timer1 [ 0.454611] NET: Registered protocol family 2 [ 0.456692] TCP established hash table entries: 2048 (order: 1, 8192 bytes) [ 0.456778] TCP bind hash table entries: 2048 (order: 1, 8192 bytes) [ 0.456852] TCP: Hash tables configured (established 2048 bind 2048) [ 0.457007] TCP: reno registered [ 0.457041] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.457090] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.457523] NET: Registered protocol family 1 [ 0.458333] RPC: Registered named UNIX socket transport module. [ 0.458361] RPC: Registered udp transport module. [ 0.458378] RPC: Registered tcp transport module. [ 0.458396] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.458430] PCI: CLS 0 bytes, default 64 [ 0.460663] hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available [ 0.467234] futex hash table entries: 256 (order: -1, 3072 bytes) [ 0.904023] VFS: Disk quotas dquot_6.5.2 [ 0.904172] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.905458] NFS: Registering the id_resolver key type [ 0.905613] Key type id_resolver registered [ 0.905635] Key type id_legacy registered [ 0.905726] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 0.906139] msgmni has been set to 485 [ 0.909736] NET: Registered protocol family 38 [ 0.909829] io scheduler noop registered [ 0.909850] io scheduler deadline registered [ 0.909901] io scheduler cfq registered (default) [ 0.913852] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568 [ 0.926010] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.933317] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@44e09000[0]' [ 0.933399] omap_uart 44e09000.serial: no wakeirq for uart0 [ 0.933431] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@44e09000[0]' [ 0.933654] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) is a OMAP UART0 [ 1.576751] console [ttyO0] enabled [ 1.581855] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@48022000[0]' [ 1.581921] omap_uart 48022000.serial: no wakeirq for uart0 [ 1.588006] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@48022000[0]' [ 1.588316] 48022000.serial: ttyO1 at MMIO 0x48022000 (irq = 89, base_baud = 3000000) is a OMAP UART1 [ 1.601221] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20 [ 1.609212] [drm] Initialized drm 1.1.0 20060810 [ 1.641622] brd: module loaded [ 1.658992] loop: module loaded [ 1.663134] (hci_tty): inside hci_tty_init [ 1.668669] (hci_tty): allocated 249, 0 [ 1.679350] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.695788] usbcore: registered new interface driver asix [ 1.702012] usbcore: registered new interface driver ax88179_178a [ 1.708854] usbcore: registered new interface driver cdc_ether [ 1.715526] usbcore: registered new interface driver smsc95xx [ 1.722037] usbcore: registered new interface driver net1080 [ 1.728441] usbcore: registered new interface driver cdc_subset [ 1.735189] usbcore: registered new interface driver zaurus [ 1.741525] usbcore: registered new interface driver cdc_ncm [ 1.748725] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 1.755653] ehci-pci: EHCI PCI platform driver [ 1.760796] ehci-omap: OMAP-EHCI Host Controller driver [ 1.767461] usbcore: registered new interface driver cdc_wdm [ 1.773960] usbcore: registered new interface driver usb-storage [ 1.782913] mousedev: PS/2 mouse device common for all mice [ 1.793530] i2c-core: driver [rtc-ds1307] using legacy suspend method [ 1.800399] i2c-core: driver [rtc-ds1307] using legacy resume method [ 1.808880] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0 [ 1.818401] i2c /dev entries driver [ 1.822466] Driver for 1-wire Dallas network protocol. [ 1.832845] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.843587] pinctrl-single 44e10800.pinmux: pin 44e109a0.0 already requested by 48022000.serial; cannot claim for 48060000.mmc [ 1.855671] pinctrl-single 44e10800.pinmux: pin-104 (48060000.mmc) status -22 [ 1.863186] pinctrl-single 44e10800.pinmux: could not request pin 104 (44e109a0.0) from group pinmux_mmc1_pins on device pinctrl-single [ 1.876102] omap_hsmmc 48060000.mmc: Error applying setting, reverse things back [ 1.884135] of_get_named_gpiod_flags exited with status 0 [ 1.884166] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@48060000[0]' [ 1.885910] pinctrl-single 44e10800.pinmux: pin 44e109a0.0 already requested by 48022000.serial; cannot claim for 48060000.mmc [ 1.897969] pinctrl-single 44e10800.pinmux: pin-104 (48060000.mmc) status -22 [ 1.905506] pinctrl-single 44e10800.pinmux: could not request pin 104 (44e109a0.0) from group pinmux_mmc1_pins on device pinctrl-single [ 1.918410] omap_hsmmc 48060000.mmc: Error applying setting, reverse things back [ 1.926230] omap_hsmmc 48060000.mmc: pins are not configured from the driver [ 1.965462] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@481d8000[0]' [ 1.965498] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@481d8000[0]' [ 2.006393] of_get_named_gpiod_flags exited with status 0 [ 2.006442] of_get_named_gpiod_flags exited with status 0 [ 2.006477] of_get_named_gpiod_flags exited with status 0 [ 2.007523] of_get_named_gpiod_flags exited with status 0 [ 2.012526] ledtrig-cpu: registered to indicate activity on CPUs [ 2.019823] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2 [ 2.032080] omap-sham 53100000.sham: hw accel on OMAP rev 4.3 [ 2.041794] usbcore: registered new interface driver usbhid [ 2.047754] usbhid: USB HID core driver [ 2.052632] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral [ 2.064848] snd-soc-dummy snd-soc-dummy: codec register snd-soc-dummy [ 2.064925] snd-soc-dummy snd-soc-dummy: component register snd-soc-dummy [ 2.065092] snd-soc-dummy snd-soc-dummy: ASoC: dai register snd-soc-dummy #1 [ 2.065131] snd-soc-dummy snd-soc-dummy: ASoC: Mapped DAI snd-soc-dummy-dai to CODEC snd-soc-dummy [ 2.065160] snd-soc-dummy snd-soc-dummy: ASoC: Registered DAI 'snd-soc-dummy-dai' [ 2.065189] snd-soc-dummy snd-soc-dummy: ASoC: Registered component 'snd-soc-dummy' [ 2.065216] snd-soc-dummy snd-soc-dummy: ASoC: Registered codec 'snd-soc-dummy' [ 2.065242] snd-soc-dummy snd-soc-dummy: ASoC: platform register snd-soc-dummy [ 2.065278] snd-soc-dummy snd-soc-dummy: ASoC: Registered platform 'snd-soc-dummy' [ 2.069129] ERMES DAVINCI EVM MCASP PROBE [ 2.069380] ERMES REGISTER DAVINCI MCASP, op_mode: 0 [ 2.069424] davinci-mcasp 48038000.mcasp: component register 48038000.mcasp [ 2.069472] davinci-mcasp 48038000.mcasp: ASoC: dai register 48038000.mcasp [ 2.069513] davinci-mcasp 48038000.mcasp: ASoC: Registered DAI '48038000.mcasp' [ 2.069542] davinci-mcasp 48038000.mcasp: ASoC: Registered component '48038000.mcasp' [ 2.069561] ERMES END REGISTER DAVINCI MCASP [ 2.069688] davinci-mcasp 48038000.mcasp: ASoC: Registered platform '48038000.mcasp' [ 2.069709] ERMES END DAVINCI MCASP PROBE [ 2.070305] INIT ERMES AM335x BOARD [ 2.070642] ERMES DAVINCI EVM PROBE [ 2.070665] device id: -1 [ 2.070681] dai name: AIC32x4 [ 2.070696] dai stream name: Playback [ 2.070861] ERMES SET SOC CARD [ 2.071000] davinci_evm sound.9: ASoC: binding AIC32x4 at idx 0 [ 2.071026] ASoC: Codec search. Compare: snd-soc-dummy and (null) [ 2.071056] davinci_evm sound.9: ASoC: CODEC (null) not registered (sigh!) [ 2.078508] mmc1: BKOPS_EN bit is not set [ 2.082995] davinci_evm sound.9: snd_soc_register_card failed (-517) [ 2.089846] platform sound.9: Driver davinci_evm requests probe deferral [ 2.098886] oprofile: using arm/armv7 [ 2.103387] TCP: cubic registered [ 2.106977] Initializing XFRM netlink socket [ 2.111898] NET: Registered protocol family 17 [ 2.116803] NET: Registered protocol family 15 [ 2.121577] mmc1: new high speed MMC card at address 0001 [ 2.127538] Key type dns_resolver registered [ 2.134801] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517 [ 2.144066] cpu cpu0: cpu0 clock notifier not ready, retry [ 2.149961] mmcblk0: mmc1:0001 MMC04G 3.60 GiB [ 2.155137] mmcblk0boot0: mmc1:0001 MMC04G partition 1 16.0 MiB [ 2.161641] mmcblk0boot1: mmc1:0001 MMC04G partition 2 16.0 MiB [ 2.167989] platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral [ 2.179322] mmcblk0: p1 p2 [ 2.182752] PM: bootloader does not support rtc-only! [ 2.190137] ThumbEE CPU extension supported. [ 2.194704] Registering SWP/SWPB emulation handler [ 2.203105] mmcblk0boot1: unknown partition table [ 2.212496] vbat: disabling [ 2.217101] regulator-dummy: disabling [ 2.221335] mmcblk0boot0: unknown partition table [ 2.235340] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 2.242320] [drm] No driver support for vblank timestamp query. [ 2.310886] Console: switching to colour frame buffer device 60x34 [ 2.323104] tilcdc 4830e000.lcdc: fb0: frame buffer device [ 2.329027] tilcdc 4830e000.lcdc: registered panic notifier [ 2.335021] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0 [ 2.348572] DCDC1: at 1500 mV [ 2.353775] vdd_mpu: 925 <--> 1375 mV at 1100 mV [ 2.360763] vdd_core: 925 <--> 1150 mV at 1100 mV [ 2.367715] LDO1: at 1800 mV [ 2.372698] LDO2: at 3300 mV [ 2.377653] LDO3: 1800 mV [ 2.382246] LDO4: at 3300 mV [ 2.387477] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 2.394572] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/i2c@44e0b000/tlv320aic32x4@18[0]' [ 2.394750] [ 2.394750] [ 2.394750] Check AIC32x4 LDO Step 1 [ 2.394830] 0-0018 supply iov not found, using dummy regulator [ 2.401332] Check AIC32x4 LDO Step 2 [ 2.401355] Check AIC32x4 LDO Step 3 [ 2.401389] tlv320aic32x4 0-0018: Missing supply 'dv' or 'ldoin' [ 2.407763] tlv320aic32x4 0-0018: Failed to setup regulators [ 2.413962] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 2.422593] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz [ 2.429938] remoteproc0: wkup_m3 is available [ 2.434637] remoteproc0: Note: remoteproc is still under development and considered experimental. [ 2.444122] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed. [ 2.455387] remoteproc0: Direct firmware load failed with error -2 [ 2.461982] remoteproc0: Falling back to user helper [ 2.468261] ERMES DAVINCI EVM PROBE [ 2.468292] device id: -1 [ 2.468309] dai name: AIC32x4 [ 2.468325] dai stream name: Playback [ 2.468498] ERMES SET SOC CARD [ 2.468613] davinci_evm sound.9: ASoC: binding AIC32x4 at idx 0 [ 2.468642] ASoC: Codec search. Compare: snd-soc-dummy and (null) [ 2.468672] davinci_evm sound.9: ASoC: CODEC (null) not registered (sigh!) [ 2.476078] davinci_evm sound.9: snd_soc_register_card failed (-517) [ 2.482812] platform sound.9: Driver davinci_evm requests probe deferral [ 2.491543] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[950000<->1100000]:-22 [ 2.555466] ERMES DAVINCI EVM PROBE [ 2.555484] device id: -1 [ 2.555494] dai name: AIC32x4 [ 2.555502] dai stream name: Playback [ 2.555625] ERMES SET SOC CARD [ 2.555706] davinci_evm sound.9: ASoC: binding AIC32x4 at idx 0 [ 2.555721] ASoC: Codec search. Compare: snd-soc-dummy and (null) [ 2.555736] davinci_evm sound.9: ASoC: CODEC (null) not registered (sigh!) [ 2.563013] davinci_evm sound.9: snd_soc_register_card failed (-517) [ 2.569780] platform sound.9: Driver davinci_evm requests probe deferral [ 2.645000] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6 [ 2.651445] davinci_mdio 4a101000.mdio: detected phy mask fffffffc [ 2.659858] ERMES DAVINCI EVM PROBE [ 2.659879] device id: -1 [ 2.659888] dai name: AIC32x4 [ 2.659897] dai stream name: Playback [ 2.660048] ERMES SET SOC CARD [ 2.660146] davinci_evm sound.9: ASoC: binding AIC32x4 at idx 0 [ 2.660164] ASoC: Codec search. Compare: snd-soc-dummy and (null) [ 2.660179] davinci_evm sound.9: ASoC: CODEC (null) not registered (sigh!) [ 2.668181] davinci_evm sound.9: snd_soc_register_card failed (-517) [ 2.674909] platform sound.9: Driver davinci_evm requests probe deferral [ 2.682202] libphy: 4a101000.mdio: probed [ 2.686465] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720 [ 2.696101] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver SMSC LAN8710/LAN8720 [ 2.706276] ERMES DAVINCI EVM PROBE [ 2.706292] device id: -1 [ 2.706301] dai name: AIC32x4 [ 2.706309] dai stream name: Playback [ 2.706428] ERMES SET SOC CARD [ 2.706499] davinci_evm sound.9: ASoC: binding AIC32x4 at idx 0 [ 2.706514] ASoC: Codec search. Compare: snd-soc-dummy and (null) [ 2.706529] davinci_evm sound.9: ASoC: CODEC (null) not registered (sigh!) [ 2.713801] davinci_evm sound.9: snd_soc_register_card failed (-517) [ 2.721632] cpsw 4a100000.ethernet: Detected MACID = 0a:11:23:32:12:88 [ 2.728712] platform sound.9: Driver davinci_evm requests probe deferral [ 2.737398] cpsw 4a100000.ethernet: cpsw: Detected MACID = 68:c9:0b:2e:62:42 [ 2.745621] ERMES DAVINCI EVM PROBE [ 2.745639] device id: -1 [ 2.745648] dai name: AIC32x4 [ 2.745656] dai stream name: Playback [ 2.745788] ERMES SET SOC CARD [ 2.745881] davinci_evm sound.9: ASoC: binding AIC32x4 at idx 0 [ 2.745896] ASoC: Codec search. Compare: snd-soc-dummy and (null) [ 2.745912] davinci_evm sound.9: ASoC: CODEC (null) not registered (sigh!) [ 2.753220] davinci_evm sound.9: snd_soc_register_card failed (-517) [ 2.762126] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) [ 2.775093] platform sound.9: Driver davinci_evm requests probe deferral [ 2.782835] ERMES DAVINCI EVM PROBE [ 2.782852] device id: -1 [ 2.782862] dai name: AIC32x4 [ 2.782869] dai stream name: Playback [ 2.783040] ERMES SET SOC CARD [ 2.783124] davinci_evm sound.9: ASoC: binding AIC32x4 at idx 0 [ 2.783143] ASoC: Codec search. Compare: snd-soc-dummy and (null) [ 2.783161] davinci_evm sound.9: ASoC: CODEC (null) not registered (sigh!) [ 2.791504] net eth0: initializing cpsw version 1.12 (0) [ 2.802705] davinci_evm sound.9: snd_soc_register_card failed (-517) [ 2.809468] platform sound.9: Driver davinci_evm requests probe deferral [ 2.875737] net eth0: phy found : id is : 0x7c0f1 [ 2.891007] net eth1: initializing cpsw version 1.12 (0) [ 2.975703] net eth1: phy found : id is : 0x7c0f1 [ 5.955529] libphy: 4a101000.mdio:00 - Link is Up - 100/Full [ 5.985008] Sending DHCP requests ., OK [ 6.045731] IP-Config: Got DHCP answer from 192.168.0.1, my address is 192.168.0.241 [ 6.050653] IP-Config: Complete: [ 6.054083] device=eth0, hwaddr=0a:11:23:32:12:88, ipaddr=192.168.0.241, mask=255.255.255.0, gw=192.168.0.1 [ 6.064876] host=192.168.0.241, domain=ermes-cctv.it, nis-domain=(none) [ 6.072322] bootserver=0.0.0.0, rootserver=192.168.0.229, rootpath= [ 6.079204] nameserver0=192.168.0.1 [ 6.083630] ALSA device list: [ 6.086792] No soundcards found. [ 6.100250] VFS: Mounted root (nfs filesystem) on device 0:14. [ 6.107283] devtmpfs: mounted [ 6.111541] Freeing unused kernel memory: 268K (c07d5000 - c0818000) [ 7.069495] udevd[846]: starting version 182 [ 7.126085] random: nonblocking pool is initialized [ 8.277663] remoteproc0: powering up wkup_m3 [ 8.320171] remoteproc0: Booting fw image am335x-pm-firmware.elf, size 154412 [ 8.467633] PM: CM3 Firmware Version = 0x190 [ 8.559775] remoteproc0: remote processor wkup_m3 is now up [ 13.145968] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 13.174366] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.