Hi,
init_completion(&data->fw_loaded);
err = request_firmware_nowait(THIS_MODULE, FW_ACTION_HOTPLUG,
FIRMWARE_NAME, &spi->dev,
GFP_KERNEL, spi, firmware_load);
if (err) {
dev_err(&spi->dev, "Firmware loading failed with %d!\n", err);
return err;
}
I have the above code snippet in the probe, everything is successful but in the firware directory I dont get any xxx directory being created.
My kernel is 2.6.37, does the above call make entries in firmware directory ? Or is that Im missing something ?
Thanks And Regards,
Mike